Post Go back to editing

LT Spice component attributes for digital parts

Product Number: LTspice

Hi. I am using a counter part from the Digital library but need to know what the "Value" parameters are. I found a some help and have used "cycles=4" for the first "Value" parameter and it works. However, the output is 1V and I would like to change that if possible.

Are there a general list of the Value parameters or as a minimum - are there a parameter I can use to change the output level?

Best regards, Jorn Holtar.



moved, form update
[edited by: lallison at 2:26 PM (GMT -5) on 27 Feb 2023]