Hi,
We're trying to deploy the LTSpice software (the MSI edition) with the All Users configuration.
Launching the installer via GUI on the device and selecting All Users works.
Deploying it in bulk (silently, etc.) via the SYSTEM account fails with the following error. The icons briefly appear on the desktop, before rolling back on failure.
Invoking remote custom action. DLL: C:\WINDOWS\Installer\MSI4967.tmp, Entrypoint: OnExpandArchConfig
MSI (s) (F4!2C) [15:51:32:795]: Product: LTspice -- The system cannot find the path specified.
C:\WINDOWS\system32\config\systemprofile\AppData\Local\LTspice\examples.zip
The system cannot find the path specified.
C:\WINDOWS\system32\config\systemprofile\AppData\Local\LTspice\examples.zip
CustomAction AI_ExpandArchConfig returned actual error code 1603 (note this may not be 100% accurate if translation happened inside sandbox)
It also fails via the GUI with the same error if the process is launched via SYSTEM.
Hi,
There are two main directories it targets: for the application and the libraries. Both expecting to find as you already found which are determined by the "user id" location. It will help us if you describe the process by which you are trying to install as the error is reflecting the attempt to use a "non existent" directory.
Okay. The process we are using to install is via an RMM tool for all users of a device.
When installing for all users on the machine, the process is running as the NT AUTHORITY\SYSTEM user account. It fails when this is the case.
If we run the installation script using a logged-in user account (we can install for just that user) or we manually log on with a local administrator account (we can install for all users).
Hi,
The LTspice installation makes use of two directories in Windows: one for the application and the second one for the libraries. Both directories are under the "user id" "%APPDATA%" ( as an example typically "C:\Users\USERNAME\AppData").
As you can see from the reported error, your process is trying to make use of a directory that does not exist. If the script is meant to provide for a given "user", it will have to be aware in the location of those directories for the individual user who will run LTspice. Be aware that LTspice and its installation are making use of "%APPDATA%" as defined by Microsoft and the previous paragraph..
Is it that your RMM tool uses "one" directory for all users? LTspice is not the type of tool that I would recommend making use of "one" directory in particular the libraries.
As I also answered bellow:
The LTspice installation makes use of two directories in Windows: one for the application and the second one for the libraries. Both directories are under the "user id" "%APPDATA%" ( as an example typically "C:\Users\USERNAME\AppData").
As you can see from the reported error, your process is trying to make use of a directory that does not exist. If the script is meant to provide for a given "user", it will have to be aware in the location of those directories for the individual user who will run LTspice. Be aware that LTspice and its installation are making use of "%APPDATA%" as defined by Microsoft and the previous paragraph.
I can also confirm with the user that this install will not work as the SYSTEM account.
We are currently working on modifying our install of LTspice to the MSI version that your company is now publishing over the older exe version. In going through the process, we have noticed the following.
As answered before. The current "msi" is built for individual users to install. It is not implemented for what you are requesting. I understand you would like to be able to install via SCCM, a feature to be considered but currently not supported.
Create an mst. Use the custom action called AI_ExpandArchRollback and set the directory to a temp folder which is accessible to all users. I was able to deploy it using MECM.
Would you be kind to explain how to do this? I use Microsoft ORCA but I am not sure how to achieve this and I'd highly appreciate if you can shed some lights. Thanks