MAX3291
Production
The MAX3291/MAX3292 high-speed RS-485/RS-422 transceivers feature driver preemphasis circuitry, which extends the distance and increases the data rate...
Datasheet
MAX3291 on Analog.com
LTC2862
Production
The LTC2862/LTC2863/LTC2864/LTC2865 are low power, 20Mbps or 250kbps RS485/RS422 transceivers operating on 3V to 5.5V supplies that feature ±60V overvoltage...
Datasheet
LTC2862 on Analog.com
Hi,
Do you have an LTspice model that can simulate the RS-485 preemphasis function?
I'm considering MAX3291 and MAX22502, but I heard that there is no LTspice model.
Best regards,
Yuya