Post Go back to editing

LTspice not writing a complete file

Category: Software
Software Version: 17.1.6

I use Google Drive for desktop quite a bit. This allows for sync'ing files between system without concern. It has a "streaming" function which access the files in real time over the network and it has an "offline" sync'ing mode where changes to the file system are local and then sync'd.  I use the latter.  I've been doing this method for various programs and designs for years.   I recently started using LTSpice and discovered that when writing to the my Google Drive (G:) files are not written in completion.

For instance., I can execute a "Save As" on this file to my local C: Documents folder and it works fine:

https://pastebin.com/ch7bGzcE

You can see all 254 lines.

However, when I write that same file to G:, it stops short. Around 100 lines:

https://pastebin.com/WHR6tqSr

Parents
  • Hi  ,

    I cannot confirm if this is an LTspice issue or not because I am using a cloud for back up as well. We use OneDrive by microsoft which supposedly the same as the google drive that you use. and I encounter no issue of similar case.

    Could it be that the connected was terminated somewhere in the middle while fetching the data from google? I can not say. But if it is a problem with LTspice application similar case should have been observed using OneDrive.

    Thank you.

    Regards,

     

Reply
  • Hi  ,

    I cannot confirm if this is an LTspice issue or not because I am using a cloud for back up as well. We use OneDrive by microsoft which supposedly the same as the google drive that you use. and I encounter no issue of similar case.

    Could it be that the connected was terminated somewhere in the middle while fetching the data from google? I can not say. But if it is a problem with LTspice application similar case should have been observed using OneDrive.

    Thank you.

    Regards,

     

Children