the figure below is my circuit:
It should do the following:
It takes the input (from 0 to 0.9v) and gives two differential outputs that are half the input (this worked)
And the second thing (which is my problem) is that the bandwidth should be 2Mhz (low pass)
What can I do to make it work? (I would like if the two resistors do it). Thanks a lot.