Post Go back to editing

LT3790 Demo circuit convergence issue

Category: Software
Product Number: LT3790
Software Version: 17.0.32.0

I'm trying to run the LT3790 demo circuit in LTSpice.

It runs fine if I leave everything as "standard" , but if I change V1 (the supply voltage) to a PWL or any other voltage source

the circuit fails to converge.

Any help appreciated.

Regards

R.Davis

Link to circuit:

www.analog.com/.../LT3790_DC2132A_TA01A.asc

Parents
  • Hi  ,

    I tried changing V1 to a PWL source with 20V at the beginning of the simulation and found this,

    If this is the convergence issue that you encounter, you can just press the ESCAPE key. this will skip the Initial DC operating point and proceed with the transient calculation. This often happen when the ckt is having difficulty finding the initial DC operating point. 

    After pressing the ESC key, I get the same result as a normal Voltage source.

    Thanks.

    Regards,

      

Reply
  • Hi  ,

    I tried changing V1 to a PWL source with 20V at the beginning of the simulation and found this,

    If this is the convergence issue that you encounter, you can just press the ESCAPE key. this will skip the Initial DC operating point and proceed with the transient calculation. This often happen when the ckt is having difficulty finding the initial DC operating point. 

    After pressing the ESC key, I get the same result as a normal Voltage source.

    Thanks.

    Regards,

      

Children
No Data