Hi team,
I tried to simulate EMC as per your technical article(https://www.analog.com/en/technical-articles/how-to-get-the-best-results-using-ltspice-part-1.html).
It shows a syntax error when adding the plot file .please check once and give a solution.
*I am attaching asc and PLT files FYR
One thing I like to do is to convert the DM and CM noise plots to dBuV with behavioral sources in the schematic. That way, it's obvious what the 500000*V... actually means and it avoids having to manually edit the plot expression each time.
Hi MTF_Walker, would you be able to explain why the input voltage source is pulsed, rather than keeping it at a regular constant 24VDC?
Hi WM604,
That's from the original article (see figure 7). It provides a short turn-on delay for the source before settling to the DC level. I'm not 100% sure, as I didn't write the original article, but it's probably there to help the simulator with convergence.
Interesting, that article I was able to follow except why the input source changes parameters like that..
Interesting, that article I was able to follow except why the input source changes parameters like that..