Post Go back to editing

Resistance value altered by solver?

Dear communitiy,

 actually I am using LTspice for the estimation of the EMC behavior of a power electronic component. Setting up the respective model for a transient simulation was basically not a problem, but I encountered a pretty strange behavior of LTSpice: In my model some of the used resistors are obviously calculated with different resistances. For example I assign 100uOhm, but the solver calculates with 5mOhm (which I did check via Ohm's law, i.e. i divided voltage drop over the respectiv resistor by its current, see picture below). The resistance value is directly assigned, so no .param statement has been used. Altering various solver settings did not provide any improvement and in the specific case, the value seems to be nailed at 5mOhm.
Did you ever encounter such a behavior in the past and could anyone provide a clou what the actual issue here could be and how to resolve it?

Unfortunately, the overall model cannot be revealed to you :/ 

 Many thanks in advance

Kind regards,
Berndinium

Parents
  • Hello everyone,

    finally resolved the problem. Issue was a totally different one, I try to put it in a nut shell: 

    If a netlist containing subcircuits is included in a project via "inc. mynetlist.net", the defined subcircuits override any hierarchically designed subcircuit (in the LTSpice schematic of the project) with the same name. Unfortunately, there is no warning or error risen by LTspice if subcircuits are accidently defined in double by this procedure.

    Kind regards
    Berndinium

Reply
  • Hello everyone,

    finally resolved the problem. Issue was a totally different one, I try to put it in a nut shell: 

    If a netlist containing subcircuits is included in a project via "inc. mynetlist.net", the defined subcircuits override any hierarchically designed subcircuit (in the LTSpice schematic of the project) with the same name. Unfortunately, there is no warning or error risen by LTspice if subcircuits are accidently defined in double by this procedure.

    Kind regards
    Berndinium

Children