Post Go back to editing

Increasing the current limit setting for LTC4281 in LTspice

The LTC4281 part has the ability to change the current limit by adjusting the sense voltage throughout the ILIM_ADJUST register. I wanted to check my circuit with an increased ILIM value with the maximum sense voltage setting of 34.4mV (ILIM_ADJUST register set to 0x11). Is there a way to adjust this in the LTspice model as I am only seeing the 12.5mV across the sense pins which is the the lowest and default setting.

Current limit setting info in datasheet:

My schematic:

As you can see I tried some parameter names (like LIMADJUST) to see if I can find the correct setting, but no luck.

Parents Reply Children
No Data