Hi all,
I have downloaded the ADA4932 model from the web. I am using the circuit as shown in the attachment.
I think it is available without being clamped, but when I run the simulation in LTspice, it is clamped as shown in the attachment.
I think this is because the ±5V operation specification (Vee +1.4 to Vss-1.4) is being applied.
Is it a bug in LTspice for this phenomenon?
BR,
Takahiro