Hi all,
I need a circuit for converting voltage to frequency using AD537JH. Here voltage is my input signal to the ad537jh and output is in the form of frequency. I have input voltage range is -1V to +1V and AD537JH should give frequency of 5Khz to 15Khz respectively. Therefore could you suggest me an example/ application circuit diagram with AD537JH(H-10A metal cap package, 10-Pin). I have followed the datasheet. But didn't get my output, please do not suggest other V to F converters because I have already purchased AD537JH.