Post Go back to editing

How can to simulate a NTC thermistor ?

Thread Summary

The user sought a SPICE model for an NTC thermistor to simulate its behavior with temperature changes. The support engineer provided a link to TDK's NTC Thermistor Library for PSpice and an example of importing and using a specific NTC model (B57211V2472J060) in LTspice. Another user suggested modeling the resistor directly in LTspice for better accuracy, especially when using a current source.
AI Generated Content

Hello,

 I need a NTC thermistor model. I searched for a spice model but I did not found it. I interesting to simulate behavior NTC with increase temperature and decrease temperature

Parents
  • O.k., the thread is already some days old. But here comes my solution:
    In NTC datasheets the R_25 (resistance at 25 °C) and the temperature coefficient B25_50 normally is given. You can feed these data in LTspice into a behavioral source. See the example below:

    You can see the plot above is exactly the R=f(t)-curve shown iin the datasheet.
    I hope I could help you.

Reply
  • O.k., the thread is already some days old. But here comes my solution:
    In NTC datasheets the R_25 (resistance at 25 °C) and the temperature coefficient B25_50 normally is given. You can feed these data in LTspice into a behavioral source. See the example below:

    You can see the plot above is exactly the R=f(t)-curve shown iin the datasheet.
    I hope I could help you.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.