Post Go back to editing

LTspice statement editor does not update, need to use edit text change to change param values

Hello, 

In LTspice I have noticed any changes I make in statement editor or simulation command panel do not get updated when I hit the okay button. Currently when I want to change a value I right click the param statement which brings up the statement editor and then I hit Escape which replaces the statement editor with the "Edit Text" window. Changes made in the Edit Text are reflected into the workspace. This isn't a huge deal but it makes changing a lot values tedious as I need to right click -> hit escape -> update value.

This is a work laptop so I don't have Admin privileges and can't get them, so if that is the probable answer cause I'll just have to deal with it.

Parents
  • Hi,

    I just tried updating my LTspice today to 17.0.33.0.

    To me it me it seems already fixed.

    I tried both editing using the table on "change param values" window as well as using the text editor located on the lower portion of the same window and it works for me.

    Regards,

    PaulDaria

Reply
  • Hi,

    I just tried updating my LTspice today to 17.0.33.0.

    To me it me it seems already fixed.

    I tried both editing using the table on "change param values" window as well as using the text editor located on the lower portion of the same window and it works for me.

    Regards,

    PaulDaria

Children