Post Go back to editing

LTspice statement editor does not update, need to use edit text change to change param values

Hello, 

In LTspice I have noticed any changes I make in statement editor or simulation command panel do not get updated when I hit the okay button. Currently when I want to change a value I right click the param statement which brings up the statement editor and then I hit Escape which replaces the statement editor with the "Edit Text" window. Changes made in the Edit Text are reflected into the workspace. This isn't a huge deal but it makes changing a lot values tedious as I need to right click -> hit escape -> update value.

This is a work laptop so I don't have Admin privileges and can't get them, so if that is the probable answer cause I'll just have to deal with it.

Parents
  • Hi JasonIndy.

    I have seen this issue as well. Changing a .tran statement does not change on the schematic (nor does it change the simulation time).

    I reinstalled and Sync Released with no success. I have flagged this up to the LTspice design team.

    I will let you know what the outcome is

    Simon Bramble

    UK Applications

  • This problem seems to have been fixed now. I have had no reply back from the LTspice crew, but the problem seems to have gone away, so I guess some magic has been happening in the background. Please let me know if the problem has gone at your end. 

    You will have to do a Sync Release to load up the software revisions

    Please let me know

    Thanks

    Simon

  • Hi, the problem doesn't seem to have been fixed. I believe I started encountering the error after the December update. I was able to edit the .step, .meas, .tran commands from the editor dialog before the update, but I am not able to do so now. I've tried Sync Release, as well as uninstalling and reinstalling, and it did not work.

Reply
  • Hi, the problem doesn't seem to have been fixed. I believe I started encountering the error after the December update. I was able to edit the .step, .meas, .tran commands from the editor dialog before the update, but I am not able to do so now. I've tried Sync Release, as well as uninstalling and reinstalling, and it did not work.

Children
No Data