Hello,
Looking at a design that uses the RH1498 in a non-standard way. The design is relying on the current limited output capability. When using the LT1498 in a PSPICE simulation, the simulation shows the OP-AMP output going into the current-limit output, but the power dissipation of the OP-AMP does not correlated with the power supply current measurements. In the simulation I see the output current of the OP-AMP is about 38mA, yet both the positive and negative supply currents are less than 3mA each. Does the PSPICE model not work for the current limited output condition? And why does the power dissipation show -465mW?