LTspice statement editor does not update, need to use edit text change to change param values

Hello, 

In LTspice I have noticed any changes I make in statement editor or simulation command panel do not get updated when I hit the okay button. Currently when I want to change a value I right click the param statement which brings up the statement editor and then I hit Escape which replaces the statement editor with the "Edit Text" window. Changes made in the Edit Text are reflected into the workspace. This isn't a huge deal but it makes changing a lot values tedious as I need to right click -> hit escape -> update value.

This is a work laptop so I don't have Admin privileges and can't get them, so if that is the probable answer cause I'll just have to deal with it.