Hi All
I would appreciate it if someone can help me with the following LTspice error.
SPICE ERROR LOG:
Error on line 3 : u1 v1 0 v2 fb vcc vee fb ad8130 Unable to find definition of model "fb" * Unknown parameter "vcc" Fatal Error: URC instance U1: Length must be positive definite.
I'm trying to simulate the summing circuit application that is shown in the AD8129/AD8130 Datasheet on page 35.
I have checked that my LTspice model pin list is in the same order as the "AD8130.cir" SUBCKT list.
SPICE NETLIST:
R1 0 FB 1K tol=1 pwr=0.1 U1 V1 0 V2 FB VCC VEE FB AD8130 V1 V1 0 SINE(0 1 1K) V2 V2 0 SINE(0 1 1K) V3 VCC 0 12 V4 VEE 0 -12 .lib ad8130.cir .tran 1m .backanno .end
I'm not sure if there is an error with the circuit or with my model. See the attached design files below.
Thank you
Updated file attached: Removed LOG.
[edited by: Lukkewaan at 9:42 PM (GMT 0) on 19 May 2020]