LTspice for Mac crashes whenever I try to put a device



I have been kept failing in upgrade/installation of LTspice XVII for Mac, but today found that I should have install it by hand (dragging the App. of the automatically mounted folder to App folder.)   After that, device and Software updates ran successfully. 

The simulations worked fine for my old schematics.  So far, so good.

However, the application crashes whenever I try to put a device.  The application begins opening a pane, and crashes immediately. 

The backtrace in "LTspice problem reports" is as follows:

---- reports starts ---------

Process:               LTspice [25895]
Path:                  /Applications/LTspice.app/Contents/MacOS/LTspice
Identifier:            LTspice
Version:               Version 0.0 (0)
Code Type:             X86-64 (Native)
Parent Process:        ??? [1]
Responsible:           LTspice [25895]
User ID:               501

Date/Time:             2019-06-01 12:40:04.405 +0900
OS Version:            Mac OS X 10.14.5 (18F132)
Report Version:        12
Anonymous UUID:        156CC1D0-40FE-C467-9BF3-E91A444E6A21


Time Awake Since Boot: 150000 seconds

System Integrity Protection: enabled

Crashed Thread:        0  Dispatch queue: com.apple.main-thread

Exception Type:        EXC_BAD_INSTRUCTION (SIGILL)
Exception Codes:       0x0000000000000001, 0x0000000000000000
Exception Note:        EXC_CORPSE_NOTIFY

Termination Signal:    Illegal instruction: 4
Termination Reason:    Namespace SIGNAL, Code 0x4
Terminating Process:   exc handler [25895]

Application Specific Information:
Crashing on exception: -[NSAlert runModal] may not be invoked inside of transaction begin/commit pair, or inside of transaction commit (usually this means it was invoked inside of a view's -drawRect: method.)

Application Specific Backtrace 1:
0   CoreFoundation                      0x00007fff2d1c9cfd __exceptionPreprocess + 256
1   libobjc.A.dylib                     0x00007fff57873a17 objc_exception_throw + 48
2   CoreFoundation                      0x00007fff2d1c9b2f +[NSException raise:format:] + 201
3   AppKit                              0x00007fff2b075451 _NSRunModal + 156
4   AppKit                              0x00007fff2ab3eccb -[NSAlert runModal] + 225
5   LTspice                             0x00000001000adf73 _Z11vMessageBoxP4CWndPKwz + 249
6   LTspice                             0x00000001000d1b2c _Z10ReadSymbolP7__sFILEP7sSymbolb + 3298
7   LTspice                             0x00000001000d0db5 _Z10LoadSymbolPKwb + 705
8   LTspice                             0x00000001000d231b _Z12LookUpSymbolPKwPbS0_ + 253
9   LTspice                             0x0000000100330ac8 -[SelectComponent FindSymbol:] + 39
10  LTspice                             0x0000000100330ca5 -[SelectComponent outlineView:objectValueForTableColumn:byItem:] + 470
11  AppKit                              0x00007fff2a8c8667 -[NSTableView preparedCellAtColumn:row:] + 473
12  AppKit                              0x00007fff2ab56265 -[NSOutlineView preparedCellAtColumn:row:] + 51
13  AppKit                              0x00007fff2a8c830b -[NSTableView _drawContentsAtRow:column:withCellFrame:] + 47
14  AppKit                              0x00007fff2ab561d1 -[NSOutlineView _drawContentsAtRow:column:withCellFrame:] + 77
15  AppKit                              0x00007fff2a8c7a92 -[NSTableView drawRow:clipRect:] + 2011
16  AppKit                              0x00007fff2a8c6e35 -[NSTableView drawRowIndexes:clipRect:] + 500
17  AppKit                              0x00007fff2ab544d0 -[NSOutlineView drawRowIndexes:clipRect:] + 98
18  AppKit                              0x00007fff2a8c4c4b -[NSTableView drawRect:] + 1320
19  AppKit                              0x00007fff2a8c141e _NSViewDrawRect + 66
20  AppKit                              0x00007fff2a8bfcac -[NSView(NSInternal) _recursive:displayRectIgnoringOpacity:inContext:shouldChangeFontReferenceColor:stopAtLayerBackedViews:] + 1627
21  AppKit                              0x00007fff2a8bf63f __46-[NSView(NSLayerKitGlue) drawLayer:inContext:]_block_invoke + 192
22  AppKit                              0x00007fff2a8bf39c -[NSView(NSLayerKitGlue) _drawViewBackingLayer:inContext:drawingHandler:] + 1720
23  AppKit                              0x00007fff2a992f04 -[_NSBackingLayerContents drawLayer:inContext:] + 164
24  QuartzCore                          0x00007fff37ba70ab -[CALayer drawInContext:] +

......snipped....

----- end of reports ----