Post Go back to editing

ADISimRF Custom parts corrupted on version upgrade

Thread Summary

The user encountered an issue after upgrading ADISimRF from 2.0.0.7 to 2.0.0.10 where custom components with a single frequency (5745 MHz) could not be used, resulting in an unhandled exception. The support engineer suggested sending the ADISimRF_Database.mdb file to diagnose the issue. The user worked around the problem by adding the parts with a new frequency and asked about removing custom parts from the database, which is currently not supported without uninstalling the software.
AI Generated Content

When I upgraded ADISimRF from 2.0.0.7 to 2.0.0.10 ADISimRF imported 11 custom components.

When I go to use any custom component and set Output Freq field it gives a dialog with following message:

"This frequency is higher than the highest available frequency in the database for this device. ADISimRF will use the highest available device data (-1MHz). More accurate data may be entered manually."

If click OK and then is gets an Unhandled exception which you can respond: Continue or Quit. There is also a button Details which gives additional info.
Continue button allows application to continue but no fields are filled and selecting new parts does not work correctly.

Note: Each custom part in previous version only had data assigned for a single frequency (5745 MHz).

Thanks

Gavin

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.