Post Go back to editing

ADAL6110-16 does not work when powered on

Category: Hardware
Product Number: ADAL6110-16

ADAL6110-16 chip does not work when powered on, We have adopted the following methods: 1. Readjust power on sequence,  3.3V and 1.8V  soft start time up to 2ms; 2.  download  the startup code after power on according to the document. After the two methods have been tried, they still fail to start work. If the chip works normally, will the chip send a chip address to MCU through SPI after power on? At present, the chip does not send any information and the chip work current is zero.

We hope to get ADI's technical support as soon as possible. Thank you!

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.