Post Go back to editing

Unable to boot zcu102 with the AD_FMCLIDAR1_EBZ system

Hello everyone,

i want to setup the AD_FMCLIDAR1_EBZ. I follow the instructions described here: https://wiki.analog.com/resources/tools-software/linux-software/embedded_arm_images and i am not able to boot my zcu102 board.

I tryed several times with the newest release (2019_R2) and also with the older version (2019_R1), but i always get the same error:

I will be very thankful for any kind of help.

Thank you in advance!

  • Could you please post the complete boot log?

    In my case boots, even if the warning from u-boot that "No boot file file" is present.

    Thank you,

    -Liviu

  • Thank you for your reponse!

    Here is the complete boot log:

    Xilinx Zynq MP First Stage Boot Loader 
    Release 2019.1   Jul 27 2021  -  12:56:36
    NOTICE:  ATF running on XCZU9EG/silicon v4/RTL5.1 at 0xfffea000
    NOTICE:  BL31: Secure code at 0x0
    NOTICE:  BL31: Non secure code at 0x8000000
    NOTICE:  BL31: v2.0(release):xilinx-v2019.2
    NOTICE:  BL31: Built : 10:19:24, Jan 13 2020
    PMUFW:  v1.1
    
    
    U-Boot 2018.01-21436-gbba91bc203 (Jan 13 2020 - 10:50:58 +0200) Xilinx ZynqMP ZCU102 rev1.0, Build: jenkins-development-build_uboot-1
    
    I2C:   ready
    DRAM:  4 GiB
    EL Level:       EL2
    Chip ID:        zu9eg
    MMC:   sdhci@ff170000: 0 (SD)
    *** Warning - bad CRC, using default environment
    
    In:    serial@ff000000
    Out:   serial@ff000000
    Err:   serial@ff000000
    Bootmode: LVL_SHFT_SD_MODE1
    Net:   ZYNQ GEM: ff0e0000, phyaddr c, interface rgmii-id
    
    Warning: ethernet@ff0e0000 using MAC address from ROM
    eth0: ethernet@ff0e0000
    Hit any key to stop autoboot:  0 
    switch to partitions #0, OK
    mmc0 is current device
    Device: sdhci@ff170000
    Manufacturer ID: 3
    OEM: 5344
    Name: SC64G 
    Tran Speed: 50000000
    Rd Block Len: 512
    SD version 3.0
    High Capacity: Yes
    Capacity: 59.5 GiB
    Bus Width: 4-bit
    Erase Group Size: 512 Bytes
    reading uEnv.txt
    407 bytes read in 16 ms (24.4 KiB/s)
    Loaded environment from uEnv.txt
    Importing environment from SD ...
    Running uenvcmd ...
    Copying Linux from SD to RAM...
    ** No boot file defined **
    reading system.dtb
    42191 bytes read in 24 ms (1.7 MiB/s)
    reading Image
    29540864 bytes read in 1949 ms (14.5 MiB/s)
    ## Flattened Device Tree blob at 04000000
       Booting using the fdt blob at 0x4000000
       Loading Device Tree to 000000000fff2000, end 000000000ffff4ce ... OK
    
    Starting kernel ...
    
    [    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
    [    0.000000] Linux version 4.19.0-g17f4223 (jenkins@romlxbuild1.adlk.analog.com) (gcc version 8.2.0 (GCC)) #1849 SMP Tue Jul 27 13:12:14 IST 2021
    [    0.000000] Machine model: ZynqMP ZCU102 Rev1.0
    [    0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8')
    [    0.000000] bootconsole [cdns0] enabled
    [    0.000000] efi: Getting EFI parameters from FDT:
    [    0.000000] efi: UEFI not found.
    [    0.000000] cma: Reserved 256 MiB at 0x0000000070000000
    [    0.000000] psci: probing for conduit method from DT.
    [    0.000000] psci: PSCIv1.1 detected in firmware.
    [    0.000000] psci: Using standard PSCI v0.2 function IDs
    [    0.000000] psci: MIGRATE_INFO_TYPE not supported.
    [    0.000000] psci: SMC Calling Convention v1.1
    [    0.000000] random: get_random_bytes called from start_kernel+0x94/0x3f8 with crng_init=0
    [    0.000000] percpu: Embedded 22 pages/cpu @(____ptrval____) s52504 r8192 d29416 u90112
    [    0.000000] Detected VIPT I-cache on CPU0
    [    0.000000] CPU features: enabling workaround for ARM erratum 845719
    [    0.000000] Speculative Store Bypass Disable mitigation not required
    [    0.000000] CPU features: detected: Kernel page table isolation (KPTI)
    [    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 1034240
    [    0.000000] Kernel command line: console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlycon rootfstype=ext4 rootwait clk_ignore_unused cpuidle.off=1 root=/dev/mmcblk0p2 rw rootwait
    [    0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes)
    [    0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes)
    [    0.000000] software IO TLB: mapped [mem 0x6bfff000-0x6ffff000] (64MB)
    [    0.000000] Memory: 3772568K/4194304K available (12860K kernel code, 1520K rwdata, 13580K rodata, 832K init, 330K bss, 159592K reserved, 262144K cma-reserved)
    [    0.000000] rcu: Hierarchical RCU implementation.
    [    0.000000] rcu:     RCU event tracing is enabled.
    [    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.
    [    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
    [    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
    [    0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000
    [    0.000000] GIC: Using split EOI/Deactivate mode
    [    0.000000] arch_timer: cp15 timer(s) running at 99.99MHz (phys).
    [    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x170f8de2d3, max_idle_ns: 440795206112 ns
    [    0.000003] sched_clock: 56 bits at 99MHz, resolution 10ns, wraps every 4398046511101ns
    [    0.008266] Console: colour dummy device 80x25
    [    0.012392] Calibrating delay loop (skipped), value calculated using timer frequency.. 199.98 BogoMIPS (lpj=399960)
    [    0.022756] pid_max: default: 32768 minimum: 301
    [    0.027449] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes)
    [    0.034012] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes)
    [    0.041788] ASID allocator initialised with 32768 entries
    [    0.046509] rcu: Hierarchical SRCU implementation.
    [    0.051554] EFI services will not be available.
    [    0.055826] smp: Bringing up secondary CPUs ...
    [    0.060486] Detected VIPT I-cache on CPU1
    [    0.060515] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
    [    0.060819] Detected VIPT I-cache on CPU2
    [    0.060839] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
    [    0.061122] Detected VIPT I-cache on CPU3
    [    0.061141] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
    [    0.061185] smp: Brought up 1 node, 4 CPUs
    [    0.095681] SMP: Total of 4 processors activated.
    [    0.100355] CPU features: detected: 32-bit EL0 Support
    [    0.106779] CPU: All CPU(s) started at EL2
    [    0.109534] alternatives: patching kernel code
    [    0.114842] devtmpfs: initialized
    [    0.122449] Registered cp15_barrier emulation handler
    [    0.122497] Registered setend emulation handler
    [    0.126847] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
    [    0.136439] futex hash table entries: 1024 (order: 4, 65536 bytes)
    [    0.148142] xor: measuring software checksum speed
    [    0.186641]    8regs     :  2375.000 MB/sec
    [    0.226669]    8regs_prefetch:  2052.000 MB/sec
    [    0.266698]    32regs    :  2724.000 MB/sec
    [    0.306726]    32regs_prefetch:  2308.000 MB/sec
    [    0.306767] xor: using function: 32regs (2724.000 MB/sec)
    [    0.311069] pinctrl core: initialized pinctrl subsystem
    [    0.316849] NET: Registered protocol family 16
    [    0.321069] audit: initializing netlink subsys (disabled)
    [    0.326089] audit: type=2000 audit(0.272:1): state=initialized audit_enabled=0 res=1
    [    0.333728] vdso: 2 pages (1 code @ (____ptrval____), 1 data @ (____ptrval____))
    [    0.333733] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
    [    0.348480] DMA: preallocated 256 KiB pool for atomic allocations
    [    0.367839] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
    [    0.436432] raid6: int64x1  gen()   445 MB/s
    [    0.504435] raid6: int64x1  xor()   451 MB/s
    [    0.572517] raid6: int64x2  gen()   679 MB/s
    [    0.640519] raid6: int64x2  xor()   599 MB/s
    [    0.708624] raid6: int64x4  gen()   981 MB/s
    [    0.776628] raid6: int64x4  xor()   737 MB/s
    [    0.844673] raid6: int64x8  gen()  1162 MB/s
    [    0.912739] raid6: int64x8  xor()   759 MB/s
    [    0.980795] raid6: neonx1   gen()   736 MB/s
    [    1.048838] raid6: neonx1   xor()   880 MB/s
    [    1.116920] raid6: neonx2   gen()  1130 MB/s
    [    1.184929] raid6: neonx2   xor()  1173 MB/s
    [    1.252977] raid6: neonx4   gen()  1479 MB/s
    [    1.321028] raid6: neonx4   xor()  1419 MB/s
    [    1.389081] raid6: neonx8   gen()  1551 MB/s
    [    1.457122] raid6: neonx8   xor()  1459 MB/s
    [    1.457160] raid6: using algorithm neonx8 gen() 1551 MB/s
    [    1.461117] raid6: .... xor() 1459 MB/s, rmw enabled
    [    1.466048] raid6: using neon recovery algorithm
    [    1.471669] SCSI subsystem initialized
    [    1.474519] usbcore: registered new interface driver usbfs
    [    1.479835] usbcore: registered new interface driver hub
    [    1.485118] usbcore: registered new device driver usb
    [    1.490270] media: Linux media interface: v0.10
    [    1.494619] videodev: Linux video capture interface: v2.00
    [    1.500092] pps_core: LinuxPPS API ver. 1 registered
    [    1.504977] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    [    1.514071] PTP clock support registered
    [    1.517972] EDAC MC: Ver: 3.0.0
    [    1.521439] zynqmp-ipi-mbox mailbox@ff990400: Probed ZynqMP IPI Mailbox driver.
    [    1.528725] jesd204: found 0 devices and 0 topologies
    [    1.533390] FPGA manager framework
    [    1.536899] Advanced Linux Sound Architecture Driver Initialized.
    [    1.543055] Bluetooth: Core ver 2.22
    [    1.546344] NET: Registered protocol family 31
    [    1.550742] Bluetooth: HCI device and connection manager initialized
    [    1.557058] Bluetooth: HCI socket layer initialized
    [    1.561901] Bluetooth: L2CAP socket layer initialized
    [    1.566929] Bluetooth: SCO socket layer initialized
    [    1.572242] clocksource: Switched to clocksource arch_sys_counter
    [    1.577902] VFS: Disk quotas dquot_6.6.0
    [    1.581757] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
    [    1.592786] NET: Registered protocol family 2
    [    1.593201] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes)
    [    1.600698] TCP established hash table entries: 32768 (order: 6, 262144 bytes)
    [    1.608035] TCP bind hash table entries: 32768 (order: 7, 524288 bytes)
    [    1.614811] TCP: Hash tables configured (established 32768 bind 32768)
    [    1.620961] UDP hash table entries: 2048 (order: 4, 65536 bytes)
    [    1.626943] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes)
    [    1.633424] NET: Registered protocol family 1
    [    1.637807] RPC: Registered named UNIX socket transport module.
    [    1.643482] RPC: Registered udp transport module.
    [    1.648149] RPC: Registered tcp transport module.
    [    1.652822] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    1.659989] hw perfevents: no interrupt-affinity property for /pmu, guessing.
    [    1.666465] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
    [    1.674871] Initialise system trusted keyrings
    [    1.678489] workingset: timestamp_bits=62 max_order=20 bucket_order=0
    [    1.685485] NFS: Registering the id_resolver key type
    [    1.689860] Key type id_resolver registered
    [    1.693999] Key type id_legacy registered
    [    1.697985] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
    [    1.704651] jffs2: version 2.2. (NAND) (SUMMARY)  © 2001-2006 Red Hat, Inc.
    [    2.793228] NET: Registered protocol family 38
    [    2.852278] Key type asymmetric registered
    [    2.852316] Asymmetric key parser 'x509' registered
    [    2.855606] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246)
    [    2.862945] io scheduler noop registered
    [    2.866831] io scheduler deadline registered
    [    2.871101] io scheduler cfq registered (default)
    [    2.875743] io scheduler mq-deadline registered
    [    2.880240] io scheduler kyber registered
    [    2.912651] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
    [    2.917228] cacheinfo: Unable to detect cache hierarchy for CPU 0
    [    2.924003] brd: module loaded
    [    2.927866] loop: module loaded
    [    2.928089] Registered mathworks_ip class
    [    2.930523] mtdoops: mtd device (mtddev=name/number) must be supplied
    [    2.936727] xilinx_spi 9c500000.axi_quad_spi: no CS gpios available
    [    2.942491] xilinx_spi 9c600000.axi_quad_spi: no CS gpios available
    [    2.949578] libphy: Fixed MDIO Bus: probed
    [    2.953715] tun: Universal TUN/TAP device driver, 1.6
    [    2.957614] CAN device driver interface
    [    2.962361] usbcore: registered new interface driver asix
    [    2.966754] usbcore: registered new interface driver ax88179_178a
    [    2.972735] usbcore: registered new interface driver cdc_ether
    [    2.978528] usbcore: registered new interface driver net1080
    [    2.984152] usbcore: registered new interface driver cdc_subset
    [    2.990036] usbcore: registered new interface driver zaurus
    [    2.995579] usbcore: registered new interface driver cdc_ncm
    [    3.001949] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
    [    3.007661] ehci-pci: EHCI PCI platform driver
    [    3.012381] usbcore: registered new interface driver uas
    [    3.017381] usbcore: registered new interface driver usb-storage
    [    3.023372] usbcore: registered new interface driver usbserial_generic
    [    3.029825] usbserial: USB Serial support registered for generic
    [    3.035795] usbcore: registered new interface driver ftdi_sio
    [    3.041501] usbserial: USB Serial support registered for FTDI USB Serial Device
    [    3.048773] usbcore: registered new interface driver upd78f0730
    [    3.054650] usbserial: USB Serial support registered for upd78f0730
    [    3.062373] rtc_zynqmp ffa60000.rtc: rtc core: registered ffa60000.rtc as rtc0
    [    3.068105] i2c /dev entries driver
    [    3.073758] usbcore: registered new interface driver uvcvideo
    [    3.077213] USB Video Class driver (1.1.1)
    [    3.082593] Bluetooth: HCI UART driver ver 2.3
    [    3.085696] Bluetooth: HCI UART protocol H4 registered
    [    3.090794] Bluetooth: HCI UART protocol BCSP registered
    [    3.096091] Bluetooth: HCI UART protocol LL registered
    [    3.101175] Bluetooth: HCI UART protocol ATH3K registered
    [    3.106556] Bluetooth: HCI UART protocol Three-wire (H5) registered
    [    3.112808] Bluetooth: HCI UART protocol Intel registered
    [    3.118149] Bluetooth: HCI UART protocol QCA registered
    [    3.123356] usbcore: registered new interface driver bcm203x
    [    3.128971] usbcore: registered new interface driver bpa10x
    [    3.134507] usbcore: registered new interface driver bfusb
    [    3.139957] usbcore: registered new interface driver btusb
    [    3.145381] Bluetooth: Generic Bluetooth SDIO driver ver 0.1
    [    3.151048] usbcore: registered new interface driver ath3k
    [    3.156718] EDAC MC: ECC not enabled
    [    3.160154] EDAC DEVICE0: Giving out device to module zynqmp-ocm-edac controller zynqmp_ocm: DEV ff960000.memory-controller (INTERRUPT)
    [    3.172455] CPUidle arm: Failed to register cpuidle driver
    [    3.177751] sdhci: Secure Digital Host Controller Interface driver
    [    3.183704] sdhci: Copyright(c) Pierre Ossman
    [    3.188028] sdhci-pltfm: SDHCI platform and OF driver helper
    [    3.194052] ledtrig-cpu: registered to indicate activity on CPUs
    [    3.199666] zynqmp_firmware_probe Platform Management API v1.1
    [    3.205420] zynqmp_firmware_probe Trustzone version v1.0
    [    3.213502] zynqmp-pinctrl firmware:zynqmp-firmware:pinctrl: zynqmp pinctrl initialized
    [    3.240964] zynqmp_clk_mux_get_parent() getparent failed for clock: lpd_wdt, ret = -22
    [    3.243678] alg: No test for xilinx-zynqmp-aes (zynqmp-aes)
    [    3.248784] zynqmp_aes zynqmp_aes: AES Successfully Registered
    [    3.248784] 
    [    3.256332] alg: No test for xilinx-keccak-384 (zynqmp-keccak-384)
    [    3.262441] alg: No test for xilinx-zynqmp-rsa (zynqmp-rsa)
    [    3.268022] usbcore: registered new interface driver usbhid
    [    3.273339] usbhid: USB HID core driver
    [    3.278652] ad7476 spi2.0: Linked as a consumer to regulator.1
    [    3.282986] ad7476 spi2.0: Dropping the link to regulator.1
    [    3.314603] axi_sysid 85000000.axi-sysid: [ad_fmclidar1_ebz] on [zcu102] git <7c86b9f84f75d6eaad0ef29a31e74b6f6f37c447> clean [2021-02-16 06:19:51] UTC
    [    3.322860] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered
    [    3.329460] usbcore: registered new interface driver snd-usb-audio
    [    3.336939] pktgen: Packet Generator for packet performance testing. Version: 2.75
    [    3.342944] Initializing XFRM netlink socket
    [    3.346883] NET: Registered protocol family 10
    [    3.351574] Segment Routing with IPv6
    [    3.354941] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
    [    3.361077] NET: Registered protocol family 17
    [    3.365157] NET: Registered protocol family 15
    [    3.369572] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
    [    3.382857] can: controller area network core (rev 20170425 abi 9)
    [    3.388624] NET: Registered protocol family 29
    [    3.393006] can: raw protocol (rev 20170425)
    [    3.397242] can: broadcast manager protocol (rev 20170425 t)
    [    3.402868] can: netlink gateway (rev 20170425) max_hops=1
    [    3.408380] Bluetooth: RFCOMM TTY layer initialized
    [    3.413168] Bluetooth: RFCOMM socket layer initialized
    [    3.418275] Bluetooth: RFCOMM ver 1.11
    [    3.421988] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
    [    3.427261] Bluetooth: BNEP filters: protocol multicast
    [    3.432453] Bluetooth: BNEP socket layer initialized
    [    3.437381] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
    [    3.443266] Bluetooth: HIDP socket layer initialized
    [    3.448303] 9pnet: Installing 9P2000 support
    [    3.452443] NET: Registered protocol family 36
    [    3.456861] Key type dns_resolver registered
    [    3.461608] registered taskstats version 1
    [    3.465157] Loading compiled-in X.509 certificates
    [    3.470237] Btrfs loaded, crc32c=crc32c-generic
    [    3.480967] ff000000.serial: ttyPS0 at MMIO 0xff000000 (irq = 41, base_baud = 6249999) is a xuartps
    [    3.490275] console [ttyPS0] enabled
    [    3.490275] console [ttyPS0] enabled
    [    3.493872] bootconsole [cdns0] disabled
    [    3.493872] bootconsole [cdns0] disabled
    [    3.501974] ff010000.serial: ttyPS1 at MMIO 0xff010000 (irq = 42, base_baud = 6249999) is a xuartps
    [    3.515306] of-fpga-region fpga-full: FPGA Region probed
    [    3.521281] nwl-pcie fd0e0000.pcie: Link is DOWN
    [    3.525928] nwl-pcie fd0e0000.pcie: host bridge /amba/pcie@fd0e0000 ranges:
    [    3.532897] nwl-pcie fd0e0000.pcie:   MEM 0xe0000000..0xefffffff -> 0xe0000000
    [    3.540118] nwl-pcie fd0e0000.pcie:   MEM 0x600000000..0x7ffffffff -> 0x600000000
    [    3.547713] nwl-pcie fd0e0000.pcie: PCI host bridge to bus 0000:00
    [    3.553894] pci_bus 0000:00: root bus resource [bus 00-ff]
    [    3.559376] pci_bus 0000:00: root bus resource [mem 0xe0000000-0xefffffff]
    [    3.566246] pci_bus 0000:00: root bus resource [mem 0x600000000-0x7ffffffff pref]
    [    3.578384] pci 0000:00:00.0: PCI bridge to [bus 01-0c]
    [    3.584375] xilinx-dpdma fd4c0000.dma: Xilinx DPDMA engine is probed
    [    3.590956] xilinx-zynqmp-dma fd500000.dma: ZynqMP DMA driver Probe success
    [    3.598068] xilinx-zynqmp-dma fd510000.dma: ZynqMP DMA driver Probe success
    [    3.605171] xilinx-zynqmp-dma fd520000.dma: ZynqMP DMA driver Probe success
    [    3.612289] xilinx-zynqmp-dma fd530000.dma: ZynqMP DMA driver Probe success
    [    3.619385] xilinx-zynqmp-dma fd540000.dma: ZynqMP DMA driver Probe success
    [    3.626496] xilinx-zynqmp-dma fd550000.dma: ZynqMP DMA driver Probe success
    [    3.633599] xilinx-zynqmp-dma fd560000.dma: ZynqMP DMA driver Probe success
    [    3.640703] xilinx-zynqmp-dma fd570000.dma: ZynqMP DMA driver Probe success
    [    3.647953] xilinx-psgtr fd400000.zynqmp_phy: Lane:1 type:8 protocol:4 pll_locked:yes
    [    3.659358] zynqmp_clk_divider_set_rate() set divider failed for spi1_ref_div1, ret = -13
    [    3.668038] xilinx-dp-snd-codec fd4a0000.zynqmp-display:zynqmp_dp_snd_codec0: Xilinx DisplayPort Sound Codec probed
    [    3.678827] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm0: Xilinx DisplayPort Sound PCM probed
    [    3.686923] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm1: Xilinx DisplayPort Sound PCM probed
    [    3.695385] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok
    [    3.707826] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok
    [    3.720522] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: Xilinx DisplayPort Sound Card probed
    [    3.730717] OF: graph: no port node found in /amba/zynqmp-display@fd4a0000
    [    3.737743] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
    [    3.744349] [drm] No driver support for vblank timestamp query.
    [    3.750333] xlnx-drm xlnx-drm.0: bound fd4a0000.zynqmp-display (ops 0xffffff8008dd2e70)
    [    3.906734] Console: switching to colour frame buffer device 160x50
    [    3.929716] zynqmp-display fd4a0000.zynqmp-display: fb0:  frame buffer device
    [    3.937083] [drm] Initialized xlnx 1.0.0 20130509 for fd4a0000.zynqmp-display on minor 0
    [    3.945186] zynqmp-display fd4a0000.zynqmp-display: ZynqMP DisplayPort Subsystem driver probed
    [    3.954241] xilinx-psgtr fd400000.zynqmp_phy: Lane:3 type:3 protocol:2 pll_locked:yes
    [    3.962128] ahci-ceva fd0c0000.ahci: AHCI 0001.0301 32 slots 2 ports 6 Gbps 0x3 impl platform mode
    [    3.971085] ahci-ceva fd0c0000.ahci: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc sds apst 
    [    3.981730] scsi host0: ahci-ceva
    [    3.985314] scsi host1: ahci-ceva
    [    3.988762] ata1: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x100 irq 37
    [    3.996676] ata2: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x180 irq 37
    [    4.005501] ad9680 spi3.0: Unrecognized CHIP_ID 0xFF
    [    4.011342] ad9528 spi4.0: spi4.0 supply vcc not found, using dummy regulator
    [    4.018530] ad9528 spi4.0: Linked as a consumer to regulator.0
    [    4.034678] iio iio:device2: SPI Read Verify failed (0xFFFFFF)
    [    4.040535] ad9528 spi4.0: Dropping the link to regulator.0
    [    4.046118] ad9528: probe of spi4.0 failed with error -5
    [    4.052097] m25p80 spi0.0: SPI-NOR-UniqueID 104400ce580c0004080025000d21c55aac
    [    4.059321] m25p80 spi0.0: found n25q512a, expected m25p80
    [    4.065000] m25p80 spi0.0: n25q512a (131072 Kbytes)
    [    4.069902] 4 fixed-partitions partitions found on MTD device spi0.0
    [    4.076255] Creating 4 MTD partitions on "spi0.0":
    [    4.081038] 0x000000000000-0x000000100000 : "qspi-fsbl-uboot"
    [    4.087273] 0x000000100000-0x000000600000 : "qspi-linux"
    [    4.092988] 0x000000600000-0x000000620000 : "qspi-device-tree"
    [    4.099213] 0x000000620000-0x000000c00000 : "qspi-rootfs"
    [    4.107132] macb ff0e0000.ethernet: Not enabling partial store and forward
    [    4.114500] libphy: MACB_mii_bus: probed
    [    4.118508] mdio_bus ff0e0000.ethernet-ffffffff: MDIO device at address 21 is missing.
    [    4.128714] TI DP83867 ff0e0000.ethernet-ffffffff:0c: attached PHY driver [TI DP83867] (mii_bus:phy_addr=ff0e0000.ethernet-ffffffff:0c, irq=POLL)
    [    4.141763] macb ff0e0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0e0000 irq 22 (00:0a:35:07:86:ac)
    [    4.151907] xilinx-axipmon ffa00000.perf-monitor: Probed Xilinx APM
    [    4.158449] xilinx-axipmon fd0b0000.perf-monitor: Probed Xilinx APM
    [    4.164951] xilinx-axipmon fd490000.perf-monitor: Probed Xilinx APM
    [    4.171462] xilinx-axipmon ffa10000.perf-monitor: Probed Xilinx APM
    [    4.179304] dwc3 fe200000.dwc3: Failed to get clk 'ref': -2
    [    4.185234] xilinx-psgtr fd400000.zynqmp_phy: Lane:2 type:0 protocol:3 pll_locked:yes
    [    4.193486] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
    [    4.198978] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
    [    4.207570] xhci-hcd xhci-hcd.0.auto: hcc params 0x0238f625 hci version 0x100 quirks 0x0000000202010810
    [    4.216978] xhci-hcd xhci-hcd.0.auto: irq 53, io mem 0xfe200000
    [    4.223120] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 4.19
    [    4.231384] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [    4.238609] usb usb1: Product: xHCI Host Controller
    [    4.243481] usb usb1: Manufacturer: Linux 4.19.0-g17f4223 xhci-hcd
    [    4.249652] usb usb1: SerialNumber: xhci-hcd.0.auto
    [    4.254888] hub 1-0:1.0: USB hub found
    [    4.258648] hub 1-0:1.0: 1 port detected
    [    4.262747] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
    [    4.268244] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
    [    4.275908] xhci-hcd xhci-hcd.0.auto: Host supports USB 3.0  SuperSpeed
    [    4.282650] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 4.19
    [    4.290915] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [    4.298128] usb usb2: Product: xHCI Host Controller
    [    4.302999] usb usb2: Manufacturer: Linux 4.19.0-g17f4223 xhci-hcd
    [    4.309168] usb usb2: SerialNumber: xhci-hcd.0.auto
    [    4.314283] hub 2-0:1.0: USB hub found
    [    4.318042] hub 2-0:1.0: 1 port detected
    [    4.318429] ata1: SATA link down (SStatus 0 SControl 330)
    [    4.323258] pca953x 0-0020: 0-0020 supply vcc not found, using dummy regulator
    [    4.327396] ata2: SATA link down (SStatus 0 SControl 330)
    [    4.334607] pca953x 0-0020: Linked as a consumer to regulator.0
    [    4.346692] GPIO line 496 (sel0) hogged as output/low
    [    4.352078] GPIO line 497 (sel1) hogged as output/high
    [    4.357553] GPIO line 498 (sel2) hogged as output/high
    [    4.363017] GPIO line 499 (sel3) hogged as output/high
    [    4.368393] pca953x 0-0021: 0-0021 supply vcc not found, using dummy regulator
    [    4.375646] pca953x 0-0021: Linked as a consumer to regulator.0
    [    4.383071] ina2xx 3-0040: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.389894] ina2xx 3-0041: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.396713] ina2xx 3-0042: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.403535] ina2xx 3-0043: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.410353] ina2xx 3-0044: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.417170] ina2xx 3-0045: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.424007] ina2xx 3-0046: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.430823] ina2xx 3-0047: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.437647] ina2xx 3-004a: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.444463] ina2xx 3-004b: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.450870] i2c i2c-0: Added multiplexed i2c bus 3
    [    4.456360] ina2xx 4-0040: power monitor ina226 (Rshunt = 2000 uOhm)
    [    4.463173] ina2xx 4-0041: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.470532] ina2xx 4-0042: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.477357] ina2xx 4-0043: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.484176] ina2xx 4-0044: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.490996] ina2xx 4-0045: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.497757] random: fast init done
    [    4.501207] ina2xx 4-0046: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.508034] ina2xx 4-0047: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.514440] i2c i2c-0: Added multiplexed i2c bus 4
    [    4.554196] i2c i2c-0: Added multiplexed i2c bus 5
    [    4.559169] i2c i2c-0: Added multiplexed i2c bus 6
    [    4.563957] pca954x 0-0075: registered 4 multiplexed busses for I2C mux pca9544
    [    4.571315] cdns-i2c ff020000.i2c: 400 kHz mmio ff020000 irq 24
    [    4.579162] at24 7-0054: 1024 byte 24c08 EEPROM, writable, 1 bytes/write
    [    4.585905] i2c i2c-1: Added multiplexed i2c bus 7
    [    4.591046] i2c i2c-1: Added multiplexed i2c bus 8
    [    4.597925] si570 9-005d: registered, current frequency 300000000 Hz
    [    4.604339] i2c i2c-1: Added multiplexed i2c bus 9
    [    4.609219] usb 1-1: new low-speed USB device number 2 using xhci-hcd
    [    4.629656] si570 10-005d: registered, current frequency 148500000 Hz
    [    4.636142] i2c i2c-1: Added multiplexed i2c bus 10
    [    4.641251] si5324 11-0069: si5328 probed
    [    4.704318] si5324 11-0069: si5328 probe successful
    [    4.709245] i2c i2c-1: Added multiplexed i2c bus 11
    [    4.714285] i2c i2c-1: Added multiplexed i2c bus 12
    [    4.719327] i2c i2c-1: Added multiplexed i2c bus 13
    [    4.724385] i2c i2c-1: Added multiplexed i2c bus 14
    [    4.729261] pca954x 1-0074: registered 8 multiplexed busses for I2C switch pca9548
    [    4.737510] ad7291: probe of 15-002f failed with error -5
    [    4.769199] i2c i2c-1: Added multiplexed i2c bus 15
    [    4.774286] i2c i2c-1: Added multiplexed i2c bus 16
    [    4.779348] i2c i2c-1: Added multiplexed i2c bus 17
    [    4.784417] i2c i2c-1: Added multiplexed i2c bus 18
    [    4.789489] i2c i2c-1: Added multiplexed i2c bus 19
    [    4.794552] i2c i2c-1: Added multiplexed i2c bus 20
    [    4.799512] usb 1-1: New USB device found, idVendor=03f0, idProduct=1198, bcdDevice= 7.04
    [    4.807698] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
    [    4.814833] usb 1-1: Product: HP USB 1000dpi Laser Mouse
    [    4.820141] usb 1-1: Manufacturer: HP
    [    4.823980] i2c i2c-1: Added multiplexed i2c bus 21
    [    4.829156] i2c i2c-1: Added multiplexed i2c bus 22
    [    4.834027] pca954x 1-0075: registered 8 multiplexed busses for I2C switch pca9548
    [    4.841648] cdns-i2c ff030000.i2c: 400 kHz mmio ff030000 irq 25
    [    4.848903] ad5064 23-000c: Linked as a consumer to regulator.2
    [    4.855159] ltc2471 23-0014: Cannot read from device.
    [    4.860227] ltc2471: probe of 23-0014 failed with error -5
    [    4.866388] cdns-wdt fd4d0000.watchdog: Xilinx Watchdog Timer with timeout 60s
    [    4.888855] input: HP HP USB 1000dpi Laser Mouse as /devices/platform/amba/ff9d0000.usb0/fe200000.dwc3/xhci-hcd.0.auto/usb1/1-1/1-1:1.0/0003:03F0:1198.0001/input/input0
    [    4.904015] hid-generic 0003:03F0:1198.0001: input: USB HID v2.00 Mouse [HP HP USB 1000dpi Laser Mouse] on usb-xhci-hcd.0.auto-1/input0
    [    4.916441] mmc0: SDHCI controller on ff170000.mmc [ff170000.mmc] using ADMA 64-bit
    [    4.928106] hid-generic 0003:03F0:1198.0002: hiddev96: USB HID v2.00 Device [HP HP USB 1000dpi Laser Mouse] on usb-xhci-hcd.0.auto-1/input1
    [    4.941358] ad7476 spi2.0: Linked as a consumer to regulator.1
    [    4.952006] input: gpio-keys as /devices/platform/gpio-keys/input/input1
    [    4.958971] rtc_zynqmp ffa60000.rtc: setting system clock to 2019-01-12 02:29:13 UTC (1547260153)
    [    4.967851] of_cfs_init
    [    4.970313] of_cfs_init: OK
    [    4.973234] cfg80211: Loading compiled-in X.509 certificates for regulatory database
    [    5.051408] mmc0: new ultra high speed SDR104 SDXC card at address aaaa
    [    5.058532] mmcblk0: mmc0:aaaa SC64G 59.5 GiB 
    [    5.066556]  mmcblk0: p1 p2 p3
    [    5.113358] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
    [    5.119891] clk: Not disabling unused clocks
    [    5.124160] ALSA device list:
    [    5.127122]   #0: DisplayPort monitor
    [    5.131100] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
    [    5.139707] cfg80211: failed to load regulatory.db
    [    5.177996] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
    [    5.186105] VFS: Mounted root (ext4 filesystem) on device 179:2.
    [    5.197253] devtmpfs: mounted
    [    5.200394] Freeing unused kernel memory: 832K
    [    5.204870] Run /sbin/init as init process
    [    5.406697] systemd[1]: System time before build time, advancing clock.
    [    5.424770] systemd[1]: systemd 241 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +GCRYPT +GNUTLS +ACL +XZ +LZ4 +SECCOMP +BLKID +ELFUTILS +KMOD -IDN2 +IDN -PCRE2 default-hierarchy=hybrid)
    [    5.446532] systemd[1]: Detected architecture arm64.
    
    Welcome to Kuiper GNU/Linux 10 (buster)!
    
    [    5.470537] systemd[1]: Set hostname to <analog>.
    [    5.478125] random: systemd: uninitialized urandom read (16 bytes read)
    [    5.484761] systemd[1]: Initializing machine ID from random generator.
    [    5.639676] systemd[1]: File /lib/systemd/system/systemd-journald.service:12 configures an IP firewall (IPAddressDeny=any), but the local system does not support BPF/cgroup based firewalling.
    [    5.656776] systemd[1]: Proceeding WITHOUT firewalling in effect! (This warning is only shown for the first loaded unit using IP firewalling.)
    [    5.778052] systemd[1]: /etc/systemd/system/tof-server.service:1: Assignment outside of section. Ignoring.
    [    5.787745] systemd[1]: /etc/systemd/system/tof-server.service:2: Assignment outside of section. Ignoring.
    [    5.945888] random: systemd: uninitialized urandom read (16 bytes read)
    [    5.959026] random: systemd: uninitialized urandom read (16 bytes read)
    [    5.965993] systemd[1]: Listening on udev Kernel Socket.
    [  OK  ] Listening on udev Kernel Socket.
    [    5.988579] systemd[1]: Listening on fsck to fsckd communication Socket.
    [  OK  ] Listening on fsck to fsckd communication Socket.
    [  OK  ] Listening on Journal Socket.
             Starting Load Kernel Modules...
             Mounting Kernel Debug File System...
             Mounting POSIX Message Queue File System...
    [  OK  ] Started Forward Password R…uests to Wall Directory Watch.
    [  OK  ] Listening on udev Control Socket.
    [  OK  ] Created slice system-systemd\x2dfsck.slice.
             Mounting Huge Pages File System...
    [  OK  ] Listening on Journal Socket (/dev/log).
    [  OK  ] Created slice User and Session Slice.
    [  OK  ] Reached target Slices.
             Mounting RPC Pipe File System...
    [  OK  ] Listening on initctl Compatibility Named Pipe.
    [  OK  ] Created slice system-serial\x2dgetty.slice.
             Starting Set the console keyboard layout...
    [  OK  ] Reached target Swap.
             Starting udev Coldplug all Devices...
    [  OK  ] Listening on Syslog Socket.
    [  OK  ] Listening on Journal Audit Socket.
             Starting Journal Service...
    [  OK  ] Created slice system-getty.slice.
             Starting Restore / save the current clock...
    [FAILED] Failed to start Load Kernel Modules.
    See 'systemctl status systemd-modules-load.service' for details.
    [  OK  ] Mounted Kernel Debug File System.
    [  OK  ] Mounted POSIX Message Queue File System.
    [  OK  ] Mounted Huge Pages File System.
    [  OK  ] Mounted RPC Pipe File System.
    [  OK  ] Started Restore / save the current clock.
    [  OK  ] Started Journal Service.
             Starting Remount Root and Kernel File Systems...
             Starting Apply Kernel Variables...
             Mounting Kernel Configuration File System...
    [  OK  ] Started Set the console keyboard layout.
    [  OK  ] Started Apply Kernel Variables.
    [  OK  ] Mounted Kernel Configuration File System.
    [  OK  ] Started Remount Root and Kernel File Systems.
             Starting Load/Save Random Seed...
             Starting Flush Journal to Persistent Storage...
             Starting Create System Users...
    [  OK  ] Started Load/Save Random Seed.
    [  OK  ] Started Flush Journal to Persistent Storage.
    [  OK  ] Started Create System Users.
    [  OK  ] Started udev Coldplug all Devices.
             Starting Helper to synchronize boot up for ifupdown...
             Starting Create Static Device Nodes in /dev...
    [  OK  ] Started Helper to synchronize boot up for ifupdown.
    [  OK  ] Started Create Static Device Nodes in /dev.
             Starting udev Kernel Device Manager...
    [  OK  ] Reached target Local File Systems (Pre).
    [  OK  ] Started udev Kernel Device Manager.
             Starting Show Plymouth Boot Screen...
    [  OK  ] Started Show Plymouth Boot Screen.
    [  OK  ] Reached target Local Encrypted Volumes.
    [  OK  ] Started Forward Password R…s to Plymouth Directory Watch.
    [  OK  ] Found device /dev/ttyPS0.
             Starting Load Kernel Modules...
    [FAILED] Failed to start Load Kernel Modules.
    See 'systemctl status systemd-modules-load.service' for details.
    [  OK  ] Found device /dev/disk/by-partuuid/004ba301-01.
    [  OK  ] Found device /dev/ttyS0.
    [  OK  ] Listening on Load/Save RF …itch Status /dev/rfkill Watch.
             Starting File System Check…isk/by-partuuid/004ba301-01...
    [  OK  ] Started File System Check Daemon to report status.
    [  OK  ] Started File System Check …/disk/by-partuuid/004ba301-01.
             Mounting /boot...
    [  OK  ] Mounted /boot.
    [  OK  ] Reached target Local File Systems.
             Starting Tell Plymouth To Write Out Runtime Data...
             Starting Preprocess NFS configuration...
             Starting Raise network interfaces...
             Starting Create Volatile Files and Directories...
             Starting Set console font and keymap...
    [  OK  ] Started Preprocess NFS configuration.
    [  OK  ] Started Tell Plymouth To Write Out Runtime Data.
    [  OK  ] Reached target NFS client services.
    [  OK  ] Reached target Remote File Systems (Pre).
    [  OK  ] Reached target Remote File Systems.
    [  OK  ] Started Set console font and keymap.
    [  OK  ] Started Create Volatile Files and Directories.
             Starting Update UTMP about System Boot/Shutdown...
             Starting Network Time Synchronization...
    [  OK  ] Started Update UTMP about System Boot/Shutdown.
             Starting Tell Plymouth To Write Out Runtime Data...
             Starting Load Kernel Modules...
    [  OK  ] Started Tell Plymouth To Write Out Runtime Data.
    [  OK  ] Started Raise network interfaces.
    [FAILED] Failed to start Load Kernel Modules.
    See 'systemctl status systemd-modules-load.service' for details.
    [  OK  ] Started Network Time Synchronization.
    [  OK  ] Reached target System Time Synchronized.
    [  OK  ] Reached target System Initialization.
    [  OK  ] Listening on triggerhappy.socket.
    [  OK  ] Listening on GPS (Global P…ioning System) Daemon Sockets.
    [  OK  ] Listening on CUPS Scheduler.
    [  OK  ] Listening on D-Bus System Message Bus Socket.
    [  OK  ] Started CUPS Scheduler.
    [  OK  ] Reached target Paths.
    [  OK  ] Started Daily Cleanup of Temporary Directories.
    [  OK  ] Started Daily man-db regeneration.
    [  OK  ] Started Daily apt download activities.
    [  OK  ] Started Daily apt upgrade and clean activities.
    [  OK  ] Started Daily rotation of log files.
    [  OK  ] Reached target Timers.
    [  OK  ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
    [  OK  ] Reached target Sockets.
    [  OK  ] Reached target Basic System.
             Starting LSB: Resize the r…ilesystem to fill partition...
             Starting Check for Raspberry Pi EEPROM updates...
             Starting triggerhappy global hotkey daemon...
    [  OK  ] Started tof-server.service.
             Starting Modem Manager...
             Starting dphys-swapfile - …unt, and delete a swap file...
             Starting Disk Manager...
             Starting System Logging Service...
             Starting rng-tools.service...
    [  OK  ] Started Manage Sound Card State (restore and store).
    [  OK  ] Started CUPS Scheduler.
             Starting dhcpcd on all interfaces...
             Starting Regenerate SSH host keys...
    [  OK  ] Started D-Bus System Message Bus.
             Starting WPA supplicant...
    [  OK  ] Started Regular background program processing daemon.
             Starting Save/Restore Sound Card State...
             Starting Login Service...
             Starting Avahi mDNS/DNS-SD Stack...
             Starting LSB: Switch to on…nless shift key is pressed)...
    [  OK  ] Started triggerhappy global hotkey daemon.
    [FAILED] Failed to start rng-tools.service.
    See 'systemctl status rng-tools.service' for details.
    [  OK  ] Started Save/Restore Sound Card State.
    [  OK  ] Reached target Sound Card.
    [  OK  ] Started Login Service.
    [  OK  ] Started System Logging Service.
    [FAILED] Failed to start Check for Raspberry Pi EEPROM updates.
    See 'systemctl status rpi-eeprom-update.service' for details.
    [  OK  ] Started dhcpcd on all interfaces.
    [  OK  ] Started Avahi mDNS/DNS-SD Stack.
    [  OK  ] Started WPA supplicant.
             Starting Authorization Manager...
    [  OK  ] Started Make remote CUPS printers available locally.
    [  OK  ] Reached target Network.
    [  OK  ] Started IIO Daemon.
             Starting Permit User Sessions...
    [  OK  ] Reached target Network is Online.
             Starting Internet superserver...
             Starting /etc/rc.local Compatibility...
             Starting HTTP based time synchronization tool...
    [  OK  ] Started Internet superserver.
    [  OK  ] Started LSB: Switch to ond…(unless shift key is pressed).
    [  OK  ] Started Permit User Sessions.
    [  OK  ] Started /etc/rc.local Compatibility.
    [  OK  ] Started HTTP based time synchronization tool.
    [  OK  ] Started LSB: Resize the ro… filesystem to fill partition.
    [  OK  ] Started Authorization Manager.
    [  OK  ] Started Modem Manager.
    [  OK  ] Started dphys-swapfile - s…mount, and delete a swap file.
             Starting Light Display Manager...
             Starting Hold until boot process finishes up...
    [  OK  ] Started Disk Manager.
    [  OK  ] Started Hold until boot process finishes up.
    [  OK  ] Started Regenerate SSH host keys.
    
    Raspbian GNU/Linux 10 analog ttyPS0
    
    analog login: root (automatic login)
    
    Linux analog 4.19.0-g17f4223 #1849 SMP Tue Jul 27 13:12:14 IST 2021 aarch64
    
    The programs included with the Debian GNU/Linux system are free software;
    the exact distribution terms for each program are described in the
    individual files in /usr/share/doc/*/copyright.
    
    Debian GNU/Linux comes with ABSOLUTELY NO WARRANTY, to the extent
    permitted by applicable law.

     and this is the output on the screen:

    Thank you!

  • As I can see, the system boots, but you do not have the video output. I suppose you connected the screen using HDMI , that is not working. Please try connecting using the Display Port.

    I've noticed in the boot log that also you encountered this error [    4.005501] ad9680 spi3.0: Unrecognized CHIP_ID 0xFF, so the FPGA is not communicating with the lidar board. I'm also investigating this issue.

    Thank you!

  • I am already using the Display Port interface, but I don’t get a output here....If I boot with a conventional ubuntu system, everything works fine and I have a video output.

    According to the FPGA and Lidar communication: I use the FMC HPC0 interface... Maybe there are some changes of the jumpers required to enable the FMC communication? In the documentation I don’t find any solution for that....

    Thank you!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.