Hi,
I'm looking for ToF or Lidar solution for AGV/ laser measuring tool.
Range: 4meters
Fov/ Beam convergent: 1° (current Garmin Lite v4 is 4° is too big when it arrives 3.5m it is already about 30cm, want to pin point)
Update Rate: 5ms /200Hz (the faster the better)
Is ADI Lidar capable of achieving this requirement? is there any solution without using FPGA? Could we use MCU instead?
Edit Notes
more detail[edited by: jiamin at 1:42 AM (GMT -4) on 21 Oct 2021]