Hi, I updated the SD boot image “23 February 2021 release candidate (2019_R2)” through Etcher.
But Etcher's check result at the end of write stage was fail.and the 32GB sd card's capacity was changed to less than 1GB.
The boot log was followed. Although there were some fail,but the linux Os started watching from the monitor.
Please confirm does it work fine?
Thanks.
U-Boot 2014.07-dirty (Nov 20 2014 - 17:07:55)
Board: Xilinx Zynq
I2C: ready
DRAM: ECC disabled 1 GiB
MMC: zynq_sdhci: 0
SF: Detected S25FL128S_64K with page size 512 Bytes, erase size 128 KiB, total 32 MiB
*** Warning - bad CRC, using default environment
In: serial
Out: serial
Err: serial
Net: Gem.e000b000
Hit any key to stop autoboot: 3 2 1 0
Device: zynq_sdhci
Manufacturer ID: ff
OEM: 0
Name: SDU1
Tran Speed: 50000000
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 29.4 GiB
Bus Width: 4-bit
reading uEnv.txt
407 bytes read in 27 ms (14.6 KiB/s)
Loaded environment from uEnv.txt
Importing environment from SD ...
Running uenvcmd ...
Copying Linux from SD to RAM...
reading uImage
6484280 bytes read in 580 ms (10.7 MiB/s)
reading devicetree.dtb
18102 bytes read in 42 ms (420.9 KiB/s)
reading uramdisk.image.gz
** Unable to read file uramdisk.image.gz **
## Booting kernel from Legacy Image at 03000000 ...
Image Name: Linux-4.19.0-ga6ef26d
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 6484216 Bytes = 6.2 MiB
Load Address: 00008000
Entry Point: 00008000
Verifying Checksum ... OK
## Flattened Device Tree blob at 02a00000
Booting using the fdt blob at 0x2a00000
Loading Kernel Image ... OK
Loading Device Tree to 1fff8000, end 1ffff6b5 ... OK
Starting kernel ...
Booting Linux on physical CPU 0x0
Linux version 4.19.0-ga6ef26d (jenkins@romlxbuild1.adlk.analog.com) (gcc version 8.2.0 (GCC)) #1104 SMP PREEMPT Fri Feb 19 15:59:18 GMT 2021
CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
OF: fdt: Machine model: Xilinx Zynq ZC706
OF: fdt: earlycon: stdout-path /amba@0/uart@E0001000 not found
Memory policy: Data cache writealloc
cma: Reserved 128 MiB at 0x38000000
random: get_random_bytes called from start_kernel+0xa0/0x404 with crng_init=0
percpu: Embedded 16 pages/cpu @(ptrval) s33548 r8192 d23796 u65536
Built 1 zonelists, mobility grouping on. Total pages: 260608
Kernel command line: console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlycon rootfstype=ext4 rootwait clk_ignore_unused cpuidle.off=1
Booting kernel: `1 invalid for parameter `cpuidle.off'
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 888444K/1048576K available (9216K kernel code, 760K rwdata, 7012K rodata, 1024K init, 163K bss, 29060K reserved, 131072K cma-reserved, 131072K highmem)
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)
lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.text : 0x(ptrval) - 0x(ptrval) (10208 kB)
.init : 0x(ptrval) - 0x(ptrval) (1024 kB)
.data : 0x(ptrval) - 0x(ptrval) ( 761 kB)
.bss : 0x(ptrval) - 0x(ptrval) ( 164 kB)
rcu: Preemptible hierarchical RCU implementation.
rcu: RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
Tasks RCU enabled.
rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
efuse mapped to (ptrval)
slcr mapped to (ptrval)
L2C: platform modifies aux control register: 0x72360000 -> 0x72760000
L2C: DT/platform modifies aux control register: 0x72360000 -> 0x72760000
L2C-310 erratum 769419 enabled
L2C-310 enabling early BRESP for Cortex-A9
L2C-310 full line of zeros enabled for Cortex-A9
L2C-310 ID prefetch enabled, offset 1 lines
L2C-310 dynamic clock gating enabled, standby mode enabled
L2C-310 cache controller enabled, 8 ways, 512 kB
L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76760001
zynq_clock_init: clkc starts at (ptrval)
Zynq clock init
sched_clock: 64 bits at 333MHz, resolution 3ns, wraps every 4398046511103ns
clocksource: arm_global_timer: mask: 0xffffffffffffffff max_cycles: 0x4ce07af025, max_idle_ns: 440795209040 ns
Switching to timer-based delay loop, resolution 3ns
clocksource: ttc_clocksource: mask: 0xffff max_cycles: 0xffff, max_idle_ns: 537538477 ns
timer #0 at (ptrval), irq=17
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 666.66 BogoMIPS (lpj=3333333)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
CPU: Testing write buffer coherency: ok
CPU0: Spectre v2: using BPIALL workaround
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x100000 - 0x100060
rcu: Hierarchical SRCU implementation.
smp: Bringing up secondary CPUs ...
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
CPU1: Spectre v2: using BPIALL workaround
smp: Brought up 1 node, 2 CPUs
SMP: Total of 2 processors activated (1333.33 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
futex hash table entries: 512 (order: 3, 32768 bytes)
pinctrl core: initialized pinctrl subsystem
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor ladder
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
zynq-ocm f800c000.ocmc: ZYNQ OCM pool: 256 KiB @ 0x(ptrval)
zynq-pinctrl 700.pinctrl: zynq pinctrl initialized
e0001000.serial: ttyPS0 at MMIO 0xe0001000 (irq = 26, base_baud = 3125000) is a xuartps
console [ttyPS0] enabled
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
media: Linux media interface: v0.10
videodev: Linux video capture interface: v2.00
jesd204: found 0 devices and 0 topologies
FPGA manager framework
Advanced Linux Sound Architecture Driver Initialized.
clocksource: Switched to clocksource arm_global_timer
NET: Registered protocol family 2
tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 6144 bytes)
TCP established hash table entries: 8192 (order: 3, 32768 bytes)
TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
UDP hash table entries: 512 (order: 2, 16384 bytes)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Registered protocol family 1
hw perfevents: no interrupt-affinity property for /pmu@f8891000, guessing.
hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
workingset: timestamp_bits=30 max_order=18 bucket_order=0
bounce: pool size: 64 pages
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
io scheduler mq-deadline registered
io scheduler kyber registered
dma-pl330 f8003000.dmac: Loaded driver for PL330 DMAC-241330
dma-pl330 f8003000.dmac: DBUFF-128x8bytes Num_Chans-8 Num_Peri-4 Num_Events-16
brd: module loaded
loop: module loaded
Registered mathworks_ip class
xilinx_spi 7c500000.axi_quad_spi: no CS gpios available
xilinx_spi 7c600000.axi_quad_spi: no CS gpios available
m25p80 spi4.0: found s25fl128s, expected n25q128a11
m25p80 spi4.0: s25fl128s (32768 Kbytes)
5 fixed-partitions partitions found on MTD device spi4.0
Creating 5 MTD partitions on "spi4.0":
0x000000000000-0x000000500000 : "boot"
0x000000500000-0x000000520000 : "bootenv"
0x000000520000-0x000000540000 : "config"
0x000000540000-0x000000fc0000 : "image"
0x000000fc0000-0x000002000000 : "spare"
MACsec IEEE 802.1AE
libphy: Fixed MDIO Bus: probed
tun: Universal TUN/TAP device driver, 1.6
libphy: MACB_mii_bus: probed
Marvell 88E1116R e000b000.ethernet-ffffffff:07: attached PHY driver [Marvell 88E1116R] (mii_bus:phy_addr=e000b000.ethernet-ffffffff:07, irq=POLL)
macb e000b000.ethernet eth0: Cadence GEM rev 0x00020118 at 0xe000b000 irq 30 (00:0a:35:00:01:22)
usbcore: registered new interface driver asix
usbcore: registered new interface driver ax88179_178a
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver net1080
usbcore: registered new interface driver cdc_subset
usbcore: registered new interface driver zaurus
usbcore: registered new interface driver cdc_ncm
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
usbcore: registered new interface driver uas
usbcore: registered new interface driver usb-storage
usbcore: registered new interface driver usbserial_generic
usbserial: USB Serial support registered for generic
usbcore: registered new interface driver ftdi_sio
usbserial: USB Serial support registered for FTDI USB Serial Device
usbcore: registered new interface driver upd78f0730
usbserial: USB Serial support registered for upd78f0730
chipidea-usb2 e0002000.usb: e0002000.usb supply vbus not found, using dummy regulator
chipidea-usb2 e0002000.usb: Linked as a consumer to regulator.0
ULPI transceiver vendor/product ID 0x0424/0x0007
Found SMSC USB3320 ULPI transceiver.
ULPI integrity check: passed.
ci_hdrc ci_hdrc.0: EHCI Host Controller
ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 4.19
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: EHCI Host Controller
usb usb1: Manufacturer: Linux 4.19.0-ga6ef26d ehci_hcd
usb usb1: SerialNumber: ci_hdrc.0
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
i2c /dev entries driver
cdns-i2c e0005000.i2c: 400 kHz mmio e0005000 irq 23
si570 2-005d: registered, current frequency 156250000 Hz
i2c i2c-1: Added multiplexed i2c bus 2
adv7511 3-0039: 3-0039 supply avdd not found, using dummy regulator
adv7511 3-0039: Linked as a consumer to regulator.0
adv7511 3-0039: 3-0039 supply dvdd not found, using dummy regulator
adv7511 3-0039: 3-0039 supply pvdd not found, using dummy regulator
adv7511 3-0039: 3-0039 supply bgvdd not found, using dummy regulator
adv7511 3-0039: 3-0039 supply dvdd-3v not found, using dummy regulator
i2c i2c-1: Added multiplexed i2c bus 3
at24 4-0054: 1024 byte 24c08 EEPROM, writable, 1 bytes/write
i2c i2c-1: Added multiplexed i2c bus 4
pca953x 5-0021: 5-0021 supply vcc not found, using dummy regulator
pca953x 5-0021: Linked as a consumer to regulator.0
i2c i2c-1: Added multiplexed i2c bus 5
rtc-pcf8563 6-0051: low voltage detected, date/time is not reliable.
rtc-pcf8563 6-0051: rtc core: registered rtc-pcf8563 as rtc0
i2c i2c-1: Added multiplexed i2c bus 6
i2c i2c-1: Added multiplexed i2c bus 7
i2c i2c-1: Added multiplexed i2c bus 8
i2c i2c-1: Added multiplexed i2c bus 9
pca954x 1-0074: registered 8 multiplexed busses for I2C switch pca9548
usbcore: registered new interface driver uvcvideo
USB Video Class driver (1.1.1)
gspca_main: v2.14.0 registered
cdns-wdt f8005000.watchdog: Xilinx Watchdog Timer with timeout 10s
Xilinx Zynq CpuIdle Driver started
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
mmc0: SDHCI controller on e0100000.mmc [e0100000.mmc] using ADMA
ledtrig-cpu: registered to indicate activity on CPUs
hidraw: raw HID events driver (C) Jiri Kosina
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
ad7476 spi3.0: Linked as a consumer to regulator.2
ad9680 spi0.0: Unrecognized CHIP_ID 0xFF
mmc0: new high speed SDHC card at address 59b4
mmcblk0: mmc0:59b4 SDU1 29.4 GiB
ltc2471 0-0014: Cannot read from device.
ltc2471: probe of 0-0014 failed with error -11
mmcblk0: p1 p2 p3
ad5064 0-000c: Linked as a consumer to regulator.3
axi_sysid 45000000.axi-sysid-0: [ad_fmclidar1_ebz] on [zc706] git <7c86b9f84f75d6eaad0ef29a31e74b6f6f37c447> clean [2021-02-15 21:50:43] UTC
fpga_manager fpga0: Xilinx Zynq FPGA Manager registered
usbcore: registered new interface driver snd-usb-audio
NET: Registered protocol family 10
Segment Routing with IPv6
sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
NET: Registered protocol family 17
NET: Registered protocol family 36
Registering SWP/SWPB emulation handler
[drm] Cannot find any crtc or sizes
[drm] Initialized axi_hdmi_drm 1.0.0 20120930 for 70e00000.axi_hdmi on minor 0
ad9528 spi1.0: spi1.0 supply vcc not found, using dummy regulator
ad9528 spi1.0: Linked as a consumer to regulator.0
iio iio:device4: SPI Read Verify failed (0xFFFFFF)
ad9528 spi1.0: Dropping the link to regulator.0
ad9528: probe of spi1.0 failed with error -5
asoc-simple-card adv7511_hdmi_snd: spdif-hifi <-> 75c00000.axi-spdif-tx mapping ok
input: gpio_keys as /devices/soc0/gpio_keys/input/input0
rtc-pcf8563 6-0051: low voltage detected, date/time is not reliable.
rtc-pcf8563 6-0051: hctosys: unable to read the hardware clock
clk: Not disabling unused clocks
ALSA device list:
#0: HDMI monitor
random: fast init done
EXT4-fs (mmcblk0p2): recovery complete
EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
VFS: Mounted root (ext4 filesystem) on device 179:2.
devtmpfs: mounted
Freeing unused kernel memory: 1024K
Run /sbin/init as init process
systemd[1]: System time before build time, advancing clock.
systemd[1]: Failed to lookup module alias 'autofs4': Function not implemented
[drm] Cannot find any crtc or sizes
systemd[1]: systemd 241 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +GCRYPT +GNUTLS +ACL +XZ +LZ4 +SECCOMP +BLKID +ELFUTILS +KMOD -IDN2 +IDN -PCRE2 default-hierarchy=hybrid)
systemd[1]: Detected architecture arm.
Welcome to [1mKuiper GNU/Linux 10 (buster)[0m!
systemd[1]: Set hostname to <analog>.
systemd[1]: File /lib/systemd/system/systemd-journald.service:12 configures an IP firewall (IPAddressDeny=any), but the local system does not support BPF/cgroup based firewalling.
systemd[1]: Proceeding WITHOUT firewalling in effect! (This warning is only shown for the first loaded unit using IP firewalling.)
systemd[1]: /etc/systemd/system/tof-server.service:1: Assignment outside of section. Ignoring.
systemd[1]: /etc/systemd/system/tof-server.service:2: Assignment outside of section. Ignoring.
random: systemd: uninitialized urandom read (16 bytes read)
random: systemd: uninitialized urandom read (16 bytes read)
systemd[1]: Created slice system-serial\x2dgetty.slice.
[[0;32m OK [0m] Created slice [0;1;39msystem-serial\x2dgetty.slice[0m.
random: systemd: uninitialized urandom read (16 bytes read)
systemd[1]: Listening on udev Control Socket.
[[0;32m OK [0m] Listening on [0;1;39mudev Control Socket[0m.
systemd[1]: Listening on fsck to fsckd communication Socket.
[[0;32m OK [0m] Listening on [0;1;39mfsck to fsckd communication Socket[0m.
[[0;32m OK [0m] Listening on [0;1;39mudev Kernel Socket[0m.
[[0;32m OK [0m] Reached target [0;1;39mSwap[0m.
[[0;32m OK [0m] Started [0;1;39mForward Password R鈥ests to Wall Directory Watch[0m.
[[0;32m OK [0m] Listening on [0;1;39minitctl Compatibility Named Pipe[0m.
[[0;32m OK [0m] Listening on [0;1;39mJournal Socket[0m.
Starting [0;1;39mLoad Kernel Modules[0m...
Starting [0;1;39mudev Coldplug all Devices[0m...
Starting [0;1;39mRestore / save the current clock[0m...
Mounting [0;1;39mRPC Pipe File System[0m...
[[0;32m OK [0m] Listening on [0;1;39mJournal Socket (/dev/log)[0m.
[[0;32m OK [0m] Listening on [0;1;39mSyslog Socket[0m.
[[0;32m OK [0m] Created slice [0;1;39msystem-systemd\x2dfsck.slice[0m.
[[0;32m OK [0m] Created slice [0;1;39msystem-getty.slice[0m.
Starting [0;1;39mJournal Service[0m...
Starting [0;1;39mSet the console keyboard layout[0m...
Mounting [0;1;39mKernel Debug File System[0m...
[[0;32m OK [0m] Created slice [0;1;39mUser and Session Slice[0m.
[[0;32m OK [0m] Reached target [0;1;39mSlices[0m.
[[0;1;31mFAILED[0m] Failed to start [0;1;39mLoad Kernel Modules[0m.
See 'systemctl status systemd-modules-load.service' for details.
[[0;32m OK [0m] Started [0;1;39mRestore / save the current clock[0m.
[[0;32m OK [0m] Started [0;1;39mJournal Service[0m.
[[0;1;31mFAILED[0m] Failed to mount [0;1;39mRPC Pipe File System[0m.
See 'systemctl status run-rpc_pipefs.mount' for details.
[[0;1;33mDEPEND[0m] Dependency failed for [0;1;39mRPC 鈥urity service for NFS server[0m.
[[0;1;33mDEPEND[0m] Dependency failed for [0;1;39mRPC 鈥ce for NFS client and server[0m.
[[0;32m OK [0m] Mounted [0;1;39mKernel Debug File System[0m.
[[0;32m OK [0m] Reached target [0;1;39mNFS client services[0m.
[[0;32m OK [0m] Reached target [0;1;39mRemote File Systems (Pre)[0m.
[[0;32m OK [0m] Reached target [0;1;39mRemote File Systems[0m.
Starting [0;1;39mRemount Root and Kernel File Systems[0m...
Starting [0;1;39mApply Kernel Variables[0m...
Mounting [0;1;39mKernel Configuration File System[0m...
[[0;32m OK [0m] Started [0;1;39mudev Coldplug all Devices[0m.
[[0;32m OK [0m] Started [0;1;39mSet the console keyboard layout[0m.
[[0;32m OK [0m] Started [0;1;39mApply Kernel Variables[0m.
[[0;32m OK [0m] Mounted [0;1;39mKernel Configuration File System[0m.
Starting [0;1;39mHelper to synchronize boot up for ifupdown[0m...
[[0;32m OK [0m] Started [0;1;39mHelper to synchronize boot up for ifupdown[0m.
[[0;32m OK [0m] Started [0;1;39mRemount Root and Kernel File Systems[0m.
Starting [0;1;39mCreate System Users[0m...
Starting [0;1;39mLoad/Save Random Seed[0m...
Starting [0;1;39mFlush Journal to Persistent Storage[0m...
[[0;32m OK [0m] Started [0;1;39mCreate System Users[0m.
[[0;32m OK [0m] Started [0;1;39mLoad/Save Random Seed[0m.
Starting [0;1;39mCreate Static Device Nodes in /dev[0m...
[[0;32m OK [0m] Started [0;1;39mFlush Journal to Persistent Storage[0m.
[[0;32m OK [0m] Started [0;1;39mCreate Static Device Nodes in /dev[0m.
[[0;32m OK [0m] Reached target [0;1;39mLocal File Systems (Pre)[0m.
Starting [0;1;39mudev Kernel Device Manager[0m...
[[0;32m OK [0m] Started [0;1;39mudev Kernel Device Manager[0m.
Starting [0;1;39mShow Plymouth Boot Screen[0m...
[[0;32m OK [0m] Started [0;1;39mShow Plymouth Boot Screen[0m.
[[0;32m OK [0m] Started [0;1;39mForward Password R鈥 to Plymouth Directory Watch[0m.
[[0;32m OK [0m] Reached target [0;1;39mLocal Encrypted Volumes[0m.
[[0m[0;31m* [0m] (1 of 4) A start job is running for /dev/serial1 (7s / 1min 30s)
M
[K[[0;1;31m*[0m[0;31m* [0m] (1 of 4) A start job is running for /dev/serial1 (8s / 1min 30s)
M
[K[[0;31m*[0;1;31m*[0m[0;31m* [0m] (1 of 4) A start job is running for /dev/serial1 (8s / 1min 30s)
M
[K[ [0;31m*[0;1;31m*[0m[0;31m* [0m] (2 of 4) A start job is running for /dev/ttyS0 (9s / 1min 30s)
M
[K[ [0;31m*[0;1;31m*[0m[0;31m* [0m] (2 of 4) A start job is running for /dev/ttyS0 (9s / 1min 30s)
M
[K[ [0;31m*[0;1;31m*[0m[0;31m*[0m] (2 of 4) A start job is running for /dev/ttyS0 (10s / 1min 30s)
M
[K[ [0;31m*[0;1;31m*[0m] (3 of 4) A start job is running for鈥uuid/18f1f9d5-01 (10s / 1min 30s)
M
[K[ [0;31m*[0m] (3 of 4) A start job is running for鈥uuid/18f1f9d5-01 (11s / 1min 30s)
M
[K[ [0;31m*[0;1;31m*[0m] (3 of 4) A start job is running for鈥uuid/18f1f9d5-01 (11s / 1min 30s)
M
[K[ [0;31m*[0;1;31m*[0m[0;31m*[0m] (4 of 4) A start job is running for /dev/ttyPS0 (12s / 1min 30s)
M
[K[ [0;31m*[0;1;31m*[0m[0;31m* [0m] (4 of 4) A start job is running for /dev/ttyPS0 (12s / 1min 30s)
M
[K[ [0;31m*[0;1;31m*[0m[0;31m* [0m] (4 of 4) A start job is running for /dev/ttyPS0 (13s / 1min 30s)
M
[K[[0;31m*[0;1;31m*[0m[0;31m* [0m] (1 of 4) A start job is running for /dev/serial1 (13s / 1min 30s)
M
[K[[0;1;31m*[0m[0;31m* [0m] (1 of 4) A start job is running for /dev/serial1 (14s / 1min 30s)
M
[K[[0m[0;31m* [0m] (1 of 4) A start job is running for /dev/serial1 (14s / 1min 30s)
M
[K[[0;1;31m*[0m[0;31m* [0m] (2 of 4) A start job is running for /dev/ttyS0 (15s / 1min 30s)
M
[K[[0;31m*[0;1;31m*[0m[0;31m* [0m] (2 of 4) A start job is running for /dev/ttyS0 (15s / 1min 30s)
M
[K[ [0;31m*[0;1;31m*[0m[0;31m* [0m] (2 of 4) A start job is running for /dev/ttyS0 (16s / 1min 30s)
M
[K[ [0;31m*[0;1;31m*[0m[0;31m* [0m] (3 of 4) A start job is running for鈥uuid/18f1f9d5-01 (16s / 1min 30s)
M
[K[ [0;31m*[0;1;31m*[0m[0;31m*[0m] (3 of 4) A start job is running for鈥uuid/18f1f9d5-01 (17s / 1min 30s)
M
[K[ [0;31m*[0;1;31m*[0m] (3 of 4) A start job is running for鈥uuid/18f1f9d5-01 (17s / 1min 30s)
M
[K[ [0;31m*[0m] (4 of 4) A start job is running for /dev/ttyPS0 (18s / 1min 30s)
M
[K[ [0;31m*[0;1;31m*[0m] (4 of 4) A start job is running for /dev/ttyPS0 (18s / 1min 30s)
M
[K[ [0;31m*[0;1;31m*[0m[0;31m*[0m] (4 of 4) A start job is running for /dev/ttyPS0 (19s / 1min 30s)
M
[K[ [0;31m*[0;1;31m*[0m[0;31m* [0m] (1 of 4) A start job is running for /dev/serial1 (19s / 1min 30s)
M
[K[ [0;31m*[0;1;31m*[0m[0;31m* [0m] (1 of 4) A start job is running for /dev/serial1 (20s / 1min 30s)
M
[K[[0;31m*[0;1;31m*[0m[0;31m* [0m] (1 of 4) A start job is running for /dev/serial1 (20s / 1min 30s)
M
[K[[0;1;31m*[0m[0;31m* [0m] (2 of 4) A start job is running for /dev/ttyS0 (21s / 1min 30s)
M
[K[[0m[0;31m* [0m] (2 of 4) A start job is running for /dev/ttyS0 (21s / 1min 30s)
M
[K[[0;1;31m*[0m[0;31m* [0m] (2 of 4) A start job is running for /dev/ttyS0 (22s / 1min 30s)
M
[K[[0;31m*[0;1;31m*[0m[0;31m* [0m] (3 of 4) A start job is running for鈥uuid/18f1f9d5-01 (22s / 1min 30s)
M
[K[ [0;31m*[0;1;31m*[0m[0;31m* [0m] (3 of 4) A start job is running for鈥uuid/18f1f9d5-01 (23s / 1min 30s)
M
[K[ [0;31m*[0;1;31m*[0m[0;31m* [0m] (3 of 4) A start job is running for鈥uuid/18f1f9d5-01 (23s / 1min 30s)
M
[K[ [0;31m*[0;1;31m*[0m[0;31m*[0m] (4 of 4) A start job is running for /dev/ttyPS0 (24s / 1min 30s)
M
[K[ [0;31m*[0;1;31m*[0m] (4 of 4) A start job is running for /dev/ttyPS0 (24s / 1min 30s)
M
[K[ [0;31m*[0m] (4 of 4) A start job is running for /dev/ttyPS0 (25s / 1min 30s)
M
[K[ [0;31m*[0;1;31m*[0m] (1 of 4) A start job is running for /dev/serial1 (25s / 1min 30s)
M
[K[ [0;31m*[0;1;31m*[0m[0;31m*[0m] (1 of 4) A start job is running for /dev/serial1 (26s / 1min 30s)
M
[K[ [0;31m*[0;1;31m*[0m[0;31m* [0m] (1 of 4) A start job is running for /dev/serial1 (26s / 1min 30s)
M
[K[ [0;31m*[0;1;31m*[0m[0;31m* [0m] (2 of 4) A start job is running for /dev/ttyS0 (27s / 1min 30s)
M
[K[[0;31m*[0;1;31m*[0m[0;31m* [0m] (2 of 4) A start job is running for /dev/ttyS0 (27s / 1min 30s)
M
[K[[0;1;31m*[0m[0;31m* [0m] (2 of 4) A start job is running for /dev/ttyS0 (28s / 1min 30s)
M
[K[[0m[0;31m* [0m] (3 of 4) A start job is running for鈥uuid/18f1f9d5-01 (28s / 1min 30s)
M
[K[[0;1;31m*[0m[0;31m* [0m] (3 of 4) A start job is running for鈥uuid/18f1f9d5-01 (29s / 1min 30s)
M
[K[[0;31m*[0;1;31m*[0m[0;31m* [0m] (3 of 4) A start job is running for鈥uuid/18f1f9d5-01 (29s / 1min 30s)
M
[K[ [0;31m*[0;1;31m*[0m[0;31m* [0m] (4 of 4) A start job is running for /dev/ttyPS0 (30s / 1min 30s)
M
[K Starting [0;1;39mLoad Kernel Modules[0m...
[K[[0;32m OK [0m] Found device [0;1;39m/dev/ttyPS0[0m.
[[0;1;31mFAILED[0m] Failed to start [0;1;39mLoad Kernel Modules[0m.
See 'systemctl status systemd-modules-load.service' for details.
[[0;32m OK [0m] Found device [0;1;39m/dev/disk/by-partuuid/18f1f9d5-01[0m.
Starting [0;1;39mFile System Check鈥sk/by-partuuid/18f1f9d5-01[0m...
[[0;32m OK [0m] Started [0;1;39mFile System Check Daemon to report status[0m.
[[0;32m OK [0m] Started [0;1;39mFile System Check 鈥disk/by-partuuid/18f1f9d5-01[0m.
Mounting [0;1;39m/boot[0m...
[[0;32m OK [0m] Mounted [0;1;39m/boot[0m.
[[0;32m OK [0m] Reached target [0;1;39mLocal File Systems[0m.
Starting [0;1;39mTell Plymouth To Write Out Runtime Data[0m...
Starting [0;1;39mPreprocess NFS configuration[0m...
Starting [0;1;39mRaise network interfaces[0m...
Starting [0;1;39mCreate Volatile Files and Directories[0m...
Starting [0;1;39mSet console font and keymap[0m...
[[0;32m OK [0m] Started [0;1;39mTell Plymouth To Write Out Runtime Data[0m.
[[0;32m OK [0m] Started [0;1;39mPreprocess NFS configuration[0m.
[[0;32m OK [0m] Started [0;1;39mSet console font and keymap[0m.
[[0;32m OK [0m] Started [0;1;39mCreate Volatile Files and Directories[0m.
Starting [0;1;39mNetwork Time Synchronization[0m...
Starting [0;1;39mUpdate UTMP about System Boot/Shutdown[0m...
[[0;32m OK [0m] Started [0;1;39mNetwork Time Synchronization[0m.
[[0;32m OK [0m] Started [0;1;39mUpdate UTMP about System Boot/Shutdown[0m.
[[0;32m OK [0m] Started [0;1;39mRaise network interfaces[0m.
Starting [0;1;39mTell Plymouth To Write Out Runtime Data[0m...
Starting [0;1;39mLoad Kernel Modules[0m...
[[0;32m OK [0m] Reached target [0;1;39mSystem Time Synchronized[0m.
[[0;32m OK [0m] Started [0;1;39mTell Plymouth To Write Out Runtime Data[0m.
[[0;1;31mFAILED[0m] Failed to start [0;1;39mLoad Kernel Modules[0m.
See 'systemctl status systemd-modules-load.service' for details.
[[0;32m OK [0m] Reached target [0;1;39mSystem Initialization[0m.
[[0;32m OK [0m] Listening on [0;1;39mCUPS Scheduler[0m.
[[0;32m OK [0m] Listening on [0;1;39mD-Bus System Message Bus Socket[0m.
[[0;32m OK [0m] Started [0;1;39mDaily Cleanup of Temporary Directories[0m.
[[0;32m OK [0m] Listening on [0;1;39mAvahi mDNS/DNS-SD Stack Activation Socket[0m.
[[0;32m OK [0m] Started [0;1;39mDaily apt download activities[0m.
[[0;32m OK [0m] Started [0;1;39mDaily apt upgrade and clean activities[0m.
[[0;32m OK [0m] Listening on [0;1;39mtriggerhappy.socket[0m.
[[0;32m OK [0m] Started [0;1;39mDaily rotation of log files[0m.
[[0;32m OK [0m] Started [0;1;39mDaily man-db regeneration[0m.
[[0;32m OK [0m] Reached target [0;1;39mTimers[0m.
[[0;32m OK [0m] Listening on [0;1;39mGPS (Global P鈥oning System) Daemon Sockets[0m.
[[0;32m OK [0m] Reached target [0;1;39mSockets[0m.
[[0;32m OK [0m] Started [0;1;39mCUPS Scheduler[0m.
[[0;32m OK [0m] Reached target [0;1;39mPaths[0m.
[[0;32m OK [0m] Reached target [0;1;39mBasic System[0m.
Starting [0;1;39mCheck for Raspberry Pi EEPROM updates[0m...
Starting [0;1;39mrng-tools.service[0m...
[[0;32m OK [0m] Started [0;1;39mRegular background program processing daemon[0m.
[[0;32m OK [0m] Started [0;1;39mtof-server.service[0m.
Starting [0;1;39mLSB: Switch to on鈥less shift key is pressed)[0m...
Starting [0;1;39mModem Manager[0m...
Starting [0;1;39mDisk Manager[0m...
[[0;32m OK [0m] Started [0;1;39mD-Bus System Message Bus[0m.
Starting [0;1;39mLogin Service[0m...
Starting [0;1;39mSystem Logging Service[0m...
Starting [0;1;39mdhcpcd on all interfaces[0m...
Starting [0;1;39mAvahi mDNS/DNS-SD Stack[0m...
[[0;32m OK [0m] Started [0;1;39mManage Sound Card State (restore and store)[0m.
Starting [0;1;39mSave/Restore Sound Card State[0m...
Starting [0;1;39mtriggerhappy global hotkey daemon[0m...
Starting [0;1;39mWPA supplicant[0m...
[[0;32m OK [0m] Started [0;1;39mCUPS Scheduler[0m.
Starting [0;1;39mdphys-swapfile - 鈥nt, and delete a swap file[0m...
[[0;32m OK [0m] Started [0;1;39mtriggerhappy global hotkey daemon[0m.
[[0;32m OK [0m] Started [0;1;39mSystem Logging Service[0m.
[[0;32m OK [0m] Started [0;1;39mCheck for Raspberry Pi EEPROM updates[0m.
[[0;1;31mFAILED[0m] Failed to start [0;1;39mrng-tools.service[0m.
See 'systemctl status rng-tools.service' for details.
[[0;32m OK [0m] Started [0;1;39mSave/Restore Sound Card State[0m.
[[0;32m OK [0m] Started [0;1;39mdhcpcd on all interfaces[0m.
[[0;32m OK [0m] Started [0;1;39mLogin Service[0m.
Starting [0;1;39mAuthorization Manager[0m...
[[0;32m OK [0m] Reached target [0;1;39mSound Card[0m.
[[0;32m OK [0m] Started [0;1;39mAvahi mDNS/DNS-SD Stack[0m.
[[0;32m OK [0m] Started [0;1;39mWPA supplicant[0m.
[[0;32m OK [0m] Reached target [0;1;39mNetwork[0m.
[[0;32m OK [0m] Started [0;1;39mIIO Daemon[0m.
Starting [0;1;39m/etc/rc.local Compatibility[0m...
Starting [0;1;39mOpenBSD Secure Shell server[0m...
Starting [0;1;39mHTTP based time synchronization tool[0m...
Starting [0;1;39mPermit User Sessions[0m...
[[0;32m OK [0m] Started [0;1;39mMake remote CUPS printers available locally[0m.
[[0;32m OK [0m] Started [0;1;39m/etc/rc.local Compatibility[0m.
[[0;32m OK [0m] Started [0;1;39mHTTP based time synchronization tool[0m.
[[0;32m OK [0m] Started [0;1;39mdphys-swapfile - s鈥ount, and delete a swap file[0m.
[[0;32m OK [0m] Started [0;1;39mPermit User Sessions[0m.
[[0;32m OK [0m] Started [0;1;39mLSB: Switch to ond鈥unless shift key is pressed)[0m.
Starting [0;1;39mHold until boot process finishes up[0m...
Starting [0;1;39mLight Display Manager[0m...
[[0;32m OK [0m] Started [0;1;39mAuthorization Manager[0m.
[[0;32m OK [0m] Started [0;1;39mOpenBSD Secure Shell server[0m.
[[0;32m OK [0m] Started [0;1;39mModem Manager[0m.
Raspbian GNU/Linux 10 analog ttyPS0
analog login: root (automatic login)
Last login: Wed Feb 24 01:09:50 GMT 2021 on ttyPS0
Linux analog 4.19.0-ga6ef26d #1104 SMP PREEMPT Fri Feb 19 15:59:18 GMT 2021 armv7l
The programs included with the Debian GNU/Linux system are free software;
the exact distribution terms for each program are described in the
individual files in /usr/share/doc/*/copyright.
Debian GNU/Linux comes with ABSOLUTELY NO WARRANTY, to the extent
permitted by applicable law.
root@analog:~#