Post Go back to editing

ad-fmclidar1-ebz

Hi! I encountered some problems when using the ad-fmclidar1-ebz evaluation kit. When configuring the 0x0550 register of ad9094 to work in test mode and output ramp or 1/0 word toggle signals, the signals received by FPGA are correct. But when ad9094 is working in normal mode to collect the signals of input channels, the signals received by FPGA always seem to be noise. FPGA can not acquire the laser echo signals. There should be no problem with the driver and the TIA output signal is also normal. I used the ZC706. I refered to the driver for ad9094 on github(github.com/.../masteand wrote the software myself. I used the JESD204B ip core in Vivado and the ILA probes connected to the ip core's outputs. I can see the echoed signals on IIO Oscilloscope, but cannot in my own software. So I think there is something wrong in my software, but I don't know what it is. Look forward for your support! Thanks!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.