Post Go back to editing

The firmware for AD-96TOF1-EBZ

I'm considering to buy a development kit of AD-96TOF1-EBZ.

In the future, I want to develop a customized board based on AD-96TOF1-EBZ.

I have read AD-96TOF1-EBZ's support page and it is written that a firmware exists in EEPROM (?)  on the board.

At that time, can I have your support to get the firmware for such a customized board ?

Parents
  • The EEPROM on the AD-96TOF1-EBZ board contains calibration data and the ADDI9036 firmware for the 3 available modes (near, medium, far)

    On EngineerZone we can answer specific questions about the ADDI9036 and the AD-96TOF1-EBZ, but cannot provide support  for developing custom firmware. Please contact your local Analog Devices or Arrow FAE for more information on how to get dedicated development support.

  • Thank you for the information.

    I want to use the same firmware as the one written in that EEPROM on AD-96TOF1-EBZ board.

    In such a case, your support team cannot provide the firmware and calibration data for me ?

  • Yes, we can provide the firmware and calibration data as they are written now in the EEPROM, but there are a few notes:

     - The  AD-96TOF1-EBZ firmware works only for this system, any changes to the system's configuration will require the firmware to change as well

    - The calibration data is specific to each AD-96TOF1-EBZ system and each system is individually calibrated at production 

Reply
  • Yes, we can provide the firmware and calibration data as they are written now in the EEPROM, but there are a few notes:

     - The  AD-96TOF1-EBZ firmware works only for this system, any changes to the system's configuration will require the firmware to change as well

    - The calibration data is specific to each AD-96TOF1-EBZ system and each system is individually calibrated at production 

Children
  • Thank you for the information.

    I understand about firmware and calibration data.

    I also think calibration data should be prepared for each system.

    Therefore, I think it's difficult to develop my custom board with no help my local Analog Devices or Arrow FAE.

     

    When I get new another questions about this topic, please let me ask you again.