Post Go back to editing

AD-FXTOF1-EBZ with RPI4

Hi,

I am evaluating the AD-FXTOF1-EBZ with Rasperberry Pi 4. and have some questions:

1. Is there any document describe the pin definition of 25 pins and 15 pins flex cables used by the camera module

2. Is the branch rpi-5.10.y workable for current rasperberry OS? Or I need to follow the document to run rpi-4.14.y instead?

3. The document said the adi9036 require the AT24 eeprom support. What's the function of AT24?

Thank you



update info
[edited by: Rick.Chen at 6:19 AM (GMT -5) on 4 Jan 2022]
Parents Reply Children
No Data