Hi,
I tried to use AD-FXTOF1-EBZ+RPi4 for ROS.
PC side is Ubuntu 18.04LTS and ROS melodic. I build it on Ubuntu and there is no error.
https://github.com/analogdevicesinc/aditof_sdk/tree/master/bindings/ros
I connect Ubuntu PC and RPi4 due to USB-Ethernet. I can see RPi4 by SSH connection.
When I run roslaunch file with target ip address from Ubuntu PC. It has error "No cameras found".
I didn't install ROS on RPi4+camera side. And there is any setup on RPi4. ToF camera + RPi4 is only start up with SD card image which is from GitHub.
If SDK ROS package can call camera control, it should work as an camera.
But, if I have to set RPi4 for control camera and ROS node, please let me know how should I do for using ROS.
Please give me your advice for ADI TOF camera for ROS.
It looks ethernet connection issue. I asked another question for demo application. If it is related issue, I hope update the software of GitHub.
Best regards,
Jun