Post Go back to editing

Aditof-Demo connect from win10 PC for AD-FXTOF1-EBZ

Hello,

I have evaluated  AD-FXTOF1-EBZ with Raspberry pi4.

All of software on RPi was OK.

But, I tried to connect AD-FXTOF1-EBZ+RPi to Windows10 PC witch is Host PC by Aditof-Demo software.

Is the function only supported AD-96TOF-EBZ?

https://wiki.analog.com/resources/eval/user-guides/ad-96tof1-ebz/ug_windows#ethernet_connection

If I can use the remote connect function from Win10/Linux for AD-FXTOF1-EBZ, please let me know how to use the software.

I'm interested in image processing on Host PC. 

Best regards,

Jun

Parents Reply Children
  • Hi Seprimiu,

    Thank you so much for your kindly comment.

    I would like to wait the update.

    Best regards,

    Jun

  • Hi Septimin,

    I tried to use aditof-demo application which is ver3.0.0 SDK on Ubuntu. And build it manually. It didn't see any error on build process. 

    However, it could not connect to ToFcamera and RPi4 from Ubuntu PC.

    Should I need to update SD card image of the RPi4 as well?

    If I need additional action for using the application, please let me know.

    Best regards,

    Jun

  • Hello Jun,

    You will have to update the sdk manually on the rpi (to use v3.0.0 as well).The easiest way is if you connect the rpi to a monitor and follow the instructions provided by the following link:
    https://github.com/analogdevicesinc/aditof_sdk/blob/master/doc/raspberrypi3/build_instructions.md

    After the update you will have to turn on the server manually by going into the build/apps/server folder and run sudo aditof-server.

    A windows installer for the camera has been uploaded as well in this release.

    Best regards,
    Septimiu.

  • Hi Septimiu,

    Thank you so much for your advice.

    I updated Raspberry pi SDK version to v3.0.0.

    For windows and Linux new version software(v3.0.0) could connect to camera over USB-Ethernet connection!!

    Thank you so much again!

    I didn't any set up after boot Raspberry pi. It looks the server application work by default.

    But, once close the aditof-demo application of the host pc. I could not connect it again. It need to reboot the raspberry pi.

    It seems to need to control server application manually.

    Does the raspberry pi OS work the server application when every boot?

    If you have any advice to control server application over Ethernet connection, it is very helpful for my evaluation.

    By the way, I had some error "git pull" command by my default setting.

    I needed to following command to pull the latest repos at "~/workspace/github/aditof_sdk".

    $git reset --hard origin/master
    $git pull origin master

    Best regards,

    Jun

  • Hi Septimiu,

    I found solution for re-connection.

    When I use close button in the application box, I could re-connect again.

    Thank you so much for your support.

    Please close the issue.

    Best regards,

    Jun

  • Hello,

    Sorry for the late reply, I am glad that you found the solution.

    Best regards,
    Septimiu.