Hello,
I am using the AD-FXTOF1-RBZ in combination with the Raspberry Pi 3 B+ and i do not get an image from the sensor.
When the application window (aditof-demo.sh) is opened the initialization in the terminal works correct. After hitting the button play in any setting of the application, there are two error-messages. First "select timeout" and seccond "Failed to get frame from device", like in the following picture.
While the application is open, you can hear a pulsed signal from the sensor and it gets on temperature. The window with the image does not open. You can not change the
settings or close the application anymore.
The following picture shows the rebuilding of the SDK. Maybe it is because of the error message in line seven.
Thanks in advance.
Dustin