Could not create TargetSensorEnumerator because SDK is not running on target.

Try to test the AD 96ToF1 - EBZ

When run the aditof-test program gets

Could not create TargetSensorEnumerator because SDK is not running on target.
I0202 15:22:54.635776  2789 usb_sensor_enumerator.cpp:85] Looking for USB connected sensors
I0202 15:22:54.704504  2789 usb_sensor_enumerator.cpp:164] Found USB capture device at: /dev/video1
I0202 15:22:54.706863  2789 usb_sensor_enumerator.cpp:168] Received the following buffer with available sensors from target: EEPROM_NAME=24c1024;EEPROM_PATH=/sys/bus/i2c/devices/0-0056/eeprom;
W0202 15:22:54.780752  2789 camera_96tof1.cpp:91] Could not find 24c1024 while looking for storage for camera AD-96TOF1-EBZ
I0202 15:22:54.781282  2789 camera_96tof1.cpp:144] Initializing camera
W0202 15:22:54.781322  2789 camera_96tof1.cpp:147] Failed to initialize! Not all sensors are available
E0202 15:22:54.781378  2789 main.cpp:238] Could not initialize camera!

Please help!