Hello,
I have a problem with Jetson Nano SD card image for AD-96TOF1-EBZ, can you help me please?
===========================================================
case #1
-------
git pull mkdir build && cd build
cmake -DJETSON=1 -DCMAKE_PREFIX_PATH="/opt/glog;/opt/protobuf;/opt/websockets" ..
make
------
Result : Build error as below
------
=====================================================================================================
case #2
git clone github.com/.../aditof_sdk cd aditof_sdk mkdir build && cd build cmake -DJETSON=1 -DCMAKE_PREFIX_PATH="/opt/glog;/opt/protobuf;/opt/websockets" ..
make
-----
Result : Built error as below
-----
analog@analog-desktop:~/workspace/github$ git clone github.com/.../aditof_sdk Cloning into 'aditof_sdk'... remote: Enumerating objects: 254, done. remote: Counting objects: 100% (254/254), done. remote: Compressing objects: 100% (179/179), done. remote: Total 7193 (delta 113), reused 156 (delta 65), pack-reused 6939 Receiving objects: 100% (7193/7193), 80.19 MiB | 370.00 KiB/s, done. Resolving deltas: 100% (4419/4419), done. analog@analog-desktop:~/workspace/github$ cd aditof_sdk analog@analog-desktop:~/workspace/github/aditof_sdk$ ls build ls: cannot access 'build': No such file or directory analog@analog-desktop:~/workspace/github/aditof_sdk$ mkdir build analog@analog-desktop:~/workspace/github/aditof_sdk$ cd build analog@analog-desktop:~/workspace/github/aditof_sdk/build$ cmake -DJETSON=1 -DCMAKE_PREFIX_PATH="/opt/glog;/opt/protobuf;/opt/websockets" .. -- The C compiler identification is GNU 7.4.0 -- The CXX compiler identification is GNU 7.4.0 -- Check for working C compiler: /usr/bin/cc -- Check for working C compiler: /usr/bin/cc -- works -- Detecting C compiler ABI info -- Detecting C compiler ABI info - done -- Detecting C compile features -- Detecting C compile features - done -- Check for working CXX compiler: /usr/bin/c++ -- Check for working CXX compiler: /usr/bin/c++ -- works -- Detecting CXX compiler ABI info -- Detecting CXX compiler ABI info - done -- Detecting CXX compile features -- Detecting CXX compile features - done -- Looking for pthread.h -- Looking for pthread.h - found -- Looking for pthread_create -- Looking for pthread_create - not found -- Looking for pthread_create in pthreads -- Looking for pthread_create in pthreads - not found -- Looking for pthread_create in pthread -- Looking for pthread_create in pthread - found -- Found Threads: TRUE -- Found Protobuf: /opt/protobuf/lib/libprotobuf.a;-lpthread (found suitable version "3.9.0", minimum required is "3.9.0") -- Found OpenCV: /usr (found version "4.1.1") -- Configuring done -- Generating done -- Build files have been written to: /home/analog/workspace/github/aditof_sdk/build analog@analog-desktop:~/workspace/github/aditof_sdk/build$ make [ 2%] Running C++ protocol buffer compiler on src/connections/network/buffer.proto Scanning dependencies of target aditof [ 4%] Building CXX object sdk/CMakeFiles/aditof.dir/src/camera_factory.cpp.o [ 6%] Building CXX object sdk/CMakeFiles/aditof.dir/src/device_enumerator_factory.cpp.o [ 8%] Building CXX object sdk/CMakeFiles/aditof.dir/src/device_enumerator_impl.cpp.o [ 10%] Building CXX object sdk/CMakeFiles/aditof.dir/src/device_factory.cpp.o [ 12%] Building CXX object sdk/CMakeFiles/aditof.dir/src/eeprom_factory.cpp.o [ 14%] Building CXX object sdk/CMakeFiles/aditof.dir/src/ethernet_device.cpp.o [ 17%] Building CXX object sdk/CMakeFiles/aditof.dir/src/ethernet_eeprom.cpp.o [ 19%] Building CXX object sdk/CMakeFiles/aditof.dir/src/filters_factory.cpp.o [ 21%] Building CXX object sdk/CMakeFiles/aditof.dir/src/frame.cpp.o [ 23%] Building CXX object sdk/CMakeFiles/aditof.dir/src/frame_impl.cpp.o [ 25%] Building CXX object sdk/CMakeFiles/aditof.dir/src/frame_operations.cpp.o [ 27%] Building CXX object sdk/CMakeFiles/aditof.dir/src/system.cpp.o [ 29%] Building CXX object sdk/CMakeFiles/aditof.dir/src/system_impl.cpp.o [ 31%] Building CXX object sdk/CMakeFiles/aditof.dir/src/usb_device.cpp.o [ 34%] Building CXX object sdk/CMakeFiles/aditof.dir/src/utils.cpp.o [ 36%] Building CXX object sdk/CMakeFiles/aditof.dir/src/variance_filter.cpp.o [ 38%] Building CXX object sdk/CMakeFiles/aditof.dir/src/connections/mipi/local_device.cpp.o In file included from /home/analog/workspace/github/aditof_sdk/sdk/src/connections/mipi/local_device.cpp:33:0: /home/analog/workspace/github/aditof_sdk/sdk/src/connections/mipi/jetson/target_definitions.h:43:20: warning: ‘TEMP_SENSOR_REPLACEMENT_DEV_PATH’ defined but not used [-Wunused-variable] static const char *TEMP_SENSOR_REPLACEMENT_DEV_PATH = ""; ^~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ /home/analog/workspace/github/aditof_sdk/sdk/src/connections/mipi/jetson/target_definitions.h:40:20: warning: ‘EEPROM_REPLACEMENT_PATH’ defined but not used [-Wunused-variable] static const char *EEPROM_REPLACEMENT_PATH = ^~~~~~~~~~~~~~~~~~~~~~~ /home/analog/workspace/github/aditof_sdk/sdk/src/connections/mipi/jetson/target_definitions.h:38:20: warning: ‘EEPROM_DEV_PATH’ defined but not used [-Wunused-variable] static const char *EEPROM_DEV_PATH = "/sys/bus/i2c/devices/6-0056/eeprom"; ^~~~~~~~~~~~~~~ /home/analog/workspace/github/aditof_sdk/sdk/src/connections/mipi/jetson/target_definitions.h:35:20: warning: ‘EEPROM_NAME’ defined but not used [-Wunused-variable] static const char *EEPROM_NAME = "24c1024"; ^~~~~~~~~~~ [ 40%] Building CXX object sdk/CMakeFiles/aditof.dir/src/connections/mipi/local_eeprom.cpp.o [ 42%] Building CXX object sdk/CMakeFiles/aditof.dir/src/connections/mipi/usb_device.cpp.o [ 44%] Building CXX object sdk/CMakeFiles/aditof.dir/src/connections/mipi/usb_eeprom.cpp.o [ 46%] Building C object sdk/CMakeFiles/aditof.dir/src/connections/mipi/temp_sensor.c.o [ 48%] Building CXX object sdk/CMakeFiles/aditof.dir/src/connections/mipi/jetson/device_enumerator_jetson.cpp.o /home/analog/workspace/github/aditof_sdk/sdk/src/connections/mipi/jetson/device_enumerator_jetson.cpp: In member function ‘virtual aditof::Status DeviceEnumeratorImpl::findDevices(std::vector<aditof::DeviceConstructionData>&)’: /home/analog/workspace/github/aditof_sdk/sdk/src/connections/mipi/jetson/device_enumerator_jetson.cpp:68:22: warning: unused variable ‘video’ [-Wunused-variable] for (const auto &video : videoPaths) { ^~~~~ In file included from /home/analog/workspace/github/aditof_sdk/sdk/src/connections/mipi/jetson/device_enumerator_jetson.cpp:33:0: /home/analog/workspace/github/aditof_sdk/sdk/src/connections/mipi/jetson/target_definitions.h: At global scope: /home/analog/workspace/github/aditof_sdk/sdk/src/connections/mipi/jetson/target_definitions.h:45:20: warning: ‘CAPTURE_DEVICE_NAME’ defined but not used [-Wunused-variable] static const char *CAPTURE_DEVICE_NAME = "vi-output, addi9036 6-0064"; ^~~~~~~~~~~~~~~~~~~ /home/analog/workspace/github/aditof_sdk/sdk/src/connections/mipi/jetson/target_definitions.h:43:20: warning: ‘TEMP_SENSOR_REPLACEMENT_DEV_PATH’ defined but not used [-Wunused-variable] static const char *TEMP_SENSOR_REPLACEMENT_DEV_PATH = ""; ^~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ /home/analog/workspace/github/aditof_sdk/sdk/src/connections/mipi/jetson/target_definitions.h:40:20: warning: ‘EEPROM_REPLACEMENT_PATH’ defined but not used [-Wunused-variable] static const char *EEPROM_REPLACEMENT_PATH = ^~~~~~~~~~~~~~~~~~~~~~~ /home/analog/workspace/github/aditof_sdk/sdk/src/connections/mipi/jetson/target_definitions.h:37:20: warning: ‘TEMP_SENSOR_DEV_PATH’ defined but not used [-Wunused-variable] static const char *TEMP_SENSOR_DEV_PATH = "/dev/i2c-6"; ^~~~~~~~~~~~~~~~~~~~ [ 51%] Building CXX object sdk/CMakeFiles/aditof.dir/src/cameras/ad-96tof1-ebz/calibration_96tof1.cpp.o [ 53%] Building CXX object sdk/CMakeFiles/aditof.dir/src/cameras/ad-96tof1-ebz/camera_96tof1.cpp.o [ 55%] Building CXX object sdk/CMakeFiles/aditof.dir/src/connections/usb/usb_utils.cpp.o [ 57%] Building CXX object sdk/CMakeFiles/aditof.dir/src/connections/network/device_enumerator_ethernet.cpp.o [ 59%] Building CXX object sdk/CMakeFiles/aditof.dir/src/connections/network/network.cpp.o [ 61%] Building CXX object sdk/CMakeFiles/aditof.dir/buffer.pb.cc.o [ 63%] Linking CXX shared library libaditof.so [ 63%] Built target aditof Scanning dependencies of target eeprom-tool [ 65%] Building CXX object tools/eeprom-tool/CMakeFiles/eeprom-tool.dir/main.cpp.o [ 68%] Building CXX object tools/eeprom-tool/CMakeFiles/eeprom-tool.dir/eeprom_tool.cpp.o [ 70%] Building CXX object tools/eeprom-tool/CMakeFiles/eeprom-tool.dir/cam96tof1_eeprom.cpp.o [ 72%] Building CXX object tools/eeprom-tool/CMakeFiles/eeprom-tool.dir/cli_helper.cpp.o [ 74%] Building CXX object tools/eeprom-tool/CMakeFiles/eeprom-tool.dir/camera_eeprom_factory.cpp.o [ 76%] Linking CXX executable eeprom-tool ../../sdk/libaditof.so.1.6.0: undefined reference to `SSL_get_ex_new_index' ../../sdk/libaditof.so.1.6.0: undefined reference to `SSL_COMP_free_compression_methods' ../../sdk/libaditof.so.1.6.0: undefined reference to `SSL_CTX_get_ex_new_index' ../../sdk/libaditof.so.1.6.0: undefined reference to `ERR_free_strings' ../../sdk/libaditof.so.1.6.0: undefined reference to `SSL_load_error_strings' ../../sdk/libaditof.so.1.6.0: undefined reference to `SSL_library_init' ../../sdk/libaditof.so.1.6.0: undefined reference to `OPENSSL_add_all_algorithms_noconf' ../../sdk/libaditof.so.1.6.0: undefined reference to `EVP_cleanup' ../../sdk/libaditof.so.1.6.0: undefined reference to `SSLv23_server_method' ../../sdk/libaditof.so.1.6.0: undefined reference to `sk_value' ../../sdk/libaditof.so.1.6.0: undefined reference to `CRYPTO_cleanup_all_ex_data' collect2: error: ld returned 1 exit status tools/eeprom-tool/CMakeFiles/eeprom-tool.dir/build.make:200: recipe for target 'tools/eeprom-tool/eeprom-tool' failed make[2]: *** [tools/eeprom-tool/eeprom-tool] Error 1 CMakeFiles/Makefile2:190: recipe for target 'tools/eeprom-tool/CMakeFiles/eeprom-tool.dir/all' failed make[1]: *** [tools/eeprom-tool/CMakeFiles/eeprom-tool.dir/all] Error 2 Makefile:129: recipe for target 'all' failed make: *** [all] Error 2 analog@analog-desktop:~/workspace/github/aditof_sdk/build$
========================================================================================================
Best regards,
H.Kashima