Hello,
I went through the documentation for this particular chip and I noticed that all parameters and connection examples are referred with a reference clock of 45MHz on pin C6 (CLI). Is it possible to feed 60MHz clock signal into pin CLI (C6)? Would this affect device operation and performance? Can you provide any advice or guidance if one would like to do so?
I have a sensor that requires such frequency for proper frame rate operation.
Any feedback would be much appreciated.
Kind Regards,
Martin Botsov
The maximum clock is 45 MHz in the data sheet, so the operation with the clock speed higher than 45 MHz is not guaranteed.
Regards,
YH