LEDs DS1-3 in rev C Camera Board for 3D TOF kit

What do the LEDs DS1-DS3 in the 3D TOF camera board indicate? I see DS1 is on when power is on via switch S2 

  • +1
    •  Analog Employees 
    on Jan 30, 2020 7:01 AM

    DS1 - indicates the camera board is powered up

    DS2 - indicates the status of the 9V supply which powers the CCD and part of the ADDI9036. The 9VDD supply turns on only after the ADDI9036 is programmed since it is controlled by the GPO3 of ADDI9036

    DS3 - indicates the status of the 5V laser supply. It turns on only after the ADDI9036 is programmed since it is controlled by the GPO4 of ADDI9036 

    -Andrei