What are the light conditions for the AD-96TOF1-EBZ?

Under what light conditions does the system work?



tags & subject
[edited by: lallison at 8:07 PM (GMT 0) on 13 Jun 2019]
Parents
  • +1
    •  Analog Employees 
    on Jun 11, 2019 1:20 PM

    Since the system uses IR light to illuminate the scene it will work both in the dark and light conditions. The VCSELs have a wavelength of 940nm making the system suitable to be operated both indoor and outdoor. IR light generated by other light sources might affect the system’s operation. 

Reply
  • +1
    •  Analog Employees 
    on Jun 11, 2019 1:20 PM

    Since the system uses IR light to illuminate the scene it will work both in the dark and light conditions. The VCSELs have a wavelength of 940nm making the system suitable to be operated both indoor and outdoor. IR light generated by other light sources might affect the system’s operation. 

Children