Post Go back to editing

Could I use AD-96TOF1-EBZ with Nvidia jetson orin nano?

Category: Hardware
Product Number: AD-96TOF1-EBZ

I have seen there is support for Nvidia jetson nano but I need to be sure I can use the orin nano.

Thanks

Edit Notes

Orin nano
[edited by: Ur30 at 2:10 PM (GMT -4) on 28 Mar 2024]
Parents
  • When integrating devices like the AD-96TOF1-EBZ with platforms such as NVIDIA Jetson Orin Nano, compatibility depends on factors like driver support, interface compatibility, and software requirements. Ensuring proper communication protocols, such as I2C or SPI, and checking if there are supported SDKs for Jetson platforms can simplify development. It’s also beneficial to explore documentation or community forums for similar use cases, as they often provide insights into potential challenges and solutions.

Reply
  • When integrating devices like the AD-96TOF1-EBZ with platforms such as NVIDIA Jetson Orin Nano, compatibility depends on factors like driver support, interface compatibility, and software requirements. Ensuring proper communication protocols, such as I2C or SPI, and checking if there are supported SDKs for Jetson platforms can simplify development. It’s also beneficial to explore documentation or community forums for similar use cases, as they often provide insights into potential challenges and solutions.

Children
No Data