Post Go back to editing

ADDI9036 datasheet discrepancy

Category: Datasheet/Specs
Product Number: ADDI9063

Hello,

On page 3, Table 1 under General Specifications, the following values for VH power supply voltages are listed: 8.73V (Min); 9.0V (Typ); 9.27V (Max). However, on page 14, Table 15 Pin Functional Descriptions, a different range of power supply voltages for pin K10 is listed: 8V to 15.5V. So, which range of voltages is the correct one? Which range of voltages should I use throughout the circuit design process?

Kind Regards,

Martin Botsov

Edit Notes

Syntax error.
[edited by: mocuZ at 4:42 AM (GMT -4) on 15 Oct 2023]

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.