Hi, my two sets of AD-96TOF1-EBZ once were able to work on windows, but now they cannot connect to window and some problems occurred. Could anyone help on this?
The software and hareware I use are:
Software: aditof-demo v3.1.0 and latest SD card image
Hareware: AD-96TOF1-EBZ, DragonBoard 410c and win 10/11
Problem 1: The logs shows that it can select among the modes, but when I press the "play", it shows "Failed to get frame from device" and the GUI is stuck there and no reponse. By the way, there is also a message "Failed FindInterface (PIN_CATEGORY_PREVIEW)", what does it mean?
I tried different PCs (win 10 or 11) and different USB ports and cables, the same problem happened. How should I solve this?
Problem 2: On another set of AD-96TOF1-EBZ, I press the S3 button and the LED DS4 cannot light up. I have tried the "Truobleshooting" in Windows User Guide but it did not work. What else should I do to solve this or locate the problem?