Post Go back to editing

Depth, Perception & Ranging Technologies > LiDAR Solutions

Category: Software

Hello,

 

I have followed the build instructions in order to compile aditof_sdk on jetson nano platform but compilation fails :

 

output compilation attached below:  

 

can you help me ?

In file included from /home/sebmenet/Sebastien_Menet/aditof_sdk/sdk/src/connections/network/network.cpp:32:0:
/home/sebmenet/Sebastien_Menet/aditof_sdk/sdk/src/connections/network/network.h:51:17: error: ‘recursive_mutex’ in namespace ‘std’ does not name a type
static std::recursive_mutex m_mutex;
^~~~~~~~~~~~~~~
/home/sebmenet/Sebastien_Menet/aditof_sdk/sdk/src/connections/network/network.cpp:72:1: error: ‘recursive_mutex’ does not name a type
recursive_mutex Network::m_mutex;
^~~~~~~~~~~~~~~
/home/sebmenet/Sebastien_Menet/aditof_sdk/sdk/src/connections/network/network.cpp: In member function ‘int Network::ServerConnect(const string&)’:
/home/sebmenet/Sebastien_Menet/aditof_sdk/sdk/src/connections/network/network.cpp:168:27: error: ‘recursive_mutex’ is not a member of ‘std’
std::unique_lock<std::recursive_mutex> mlock(m_mutex);
^~~~~~~~~~~~~~~
/home/sebmenet/Sebastien_Menet/aditof_sdk/sdk/src/connections/network/network.cpp:168:27: error: ‘recursive_mutex’ is not a member of ‘std’
/home/sebmenet/Sebastien_Menet/aditof_sdk/sdk/src/connections/network/network.cpp:168:42: error: template argument 1 is invalid
std::unique_lock<std::recursive_mutex> mlock(m_mutex);
^
/home/sebmenet/Sebastien_Menet/aditof_sdk/sdk/src/connections/network/network.cpp:168:50: error: ‘m_mutex’ was not declared in this scope
std::unique_lock<std::recursive_mutex> mlock(m_mutex);
^~~~~~~
/home/sebmenet/Sebastien_Menet/aditof_sdk/sdk/src/connections/network/network.cpp: In member function ‘int Network::SendCommand()’:
/home/sebmenet/Sebastien_Menet/aditof_sdk/sdk/src/connections/network/network.cpp:214:34: warning: ‘int google::protobuf::MessageLite::ByteSize() const’ is deprecated: Please use ByteSizeLong() instead [-Wdeprecated-declarations]
int siz = send_buff.ByteSize();
^
In file included from /usr/local/include/google/protobuf/any.h:38:0,
from /usr/local/include/google/protobuf/generated_message_util.h:53,
from /home/sebmenet/Sebastien_Menet/aditof_sdk/build/sdk/buffer.pb.h:27,
from /home/sebmenet/Sebastien_Menet/aditof_sdk/sdk/src/connections/network/network.h:32,
from /home/sebmenet/Sebastien_Menet/aditof_sdk/sdk/src/connections/network/network.cpp:32:
/usr/local/include/google/protobuf/message_lite.h:421:7: note: declared here
int ByteSize() const { return internal::ToIntSize(ByteSizeLong()); }
^~~~~~~~
/home/sebmenet/Sebastien_Menet/aditof_sdk/sdk/src/connections/network/network.cpp:222:31: error: ‘recursive_mutex’ is not a member of ‘std’
std::unique_lock<std::recursive_mutex> mlock(m_mutex);
^~~~~~~~~~~~~~~
/home/sebmenet/Sebastien_Menet/aditof_sdk/sdk/src/connections/network/network.cpp:222:31: error: ‘recursive_mutex’ is not a member of ‘std’
/home/sebmenet/Sebastien_Menet/aditof_sdk/sdk/src/connections/network/network.cpp:222:46: error: template argument 1 is invalid
std::unique_lock<std::recursive_mutex> mlock(m_mutex);
^
/home/sebmenet/Sebastien_Menet/aditof_sdk/sdk/src/connections/network/network.cpp:222:54: error: ‘m_mutex’ was not declared in this scope
std::unique_lock<std::recursive_mutex> mlock(m_mutex);
^~~~~~~
/home/sebmenet/Sebastien_Menet/aditof_sdk/sdk/src/connections/network/network.cpp: In static member function ‘static int Network::callback_function(lws*, lws_callback_reasons, void*, void*, size_t)’:
/home/sebmenet/Sebastien_Menet/aditof_sdk/sdk/src/connections/network/network.cpp:360:30: error: ‘recursive_mutex’ is not a member of ‘std’
std::lock_guard<std::recursive_mutex> guard(m_mutex);
^~~~~~~~~~~~~~~
/home/sebmenet/Sebastien_Menet/aditof_sdk/sdk/src/connections/network/network.cpp:360:30: error: ‘recursive_mutex’ is not a member of ‘std’
/home/sebmenet/Sebastien_Menet/aditof_sdk/sdk/src/connections/network/network.cpp:360:45: error: template argument 1 is invalid
std::lock_guard<std::recursive_mutex> guard(m_mutex);
^
/home/sebmenet/Sebastien_Menet/aditof_sdk/sdk/src/connections/network/network.cpp:360:53: error: ‘m_mutex’ was not declared in this scope
std::lock_guard<std::recursive_mutex> guard(m_mutex);
^~~~~~~
/home/sebmenet/Sebastien_Menet/aditof_sdk/sdk/src/connections/network/network.cpp:360:47: warning: unused variable ‘guard’ [-Wunused-variable]
std::lock_guard<std::recursive_mutex> guard(m_mutex);
^~~~~
/home/sebmenet/Sebastien_Menet/aditof_sdk/sdk/src/connections/network/network.cpp:420:30: error: ‘recursive_mutex’ is not a member of ‘std’
std::lock_guard<std::recursive_mutex> guard(m_mutex);
^~~~~~~~~~~~~~~
/home/sebmenet/Sebastien_Menet/aditof_sdk/sdk/src/connections/network/network.cpp:420:30: error: ‘recursive_mutex’ is not a member of ‘std’
/home/sebmenet/Sebastien_Menet/aditof_sdk/sdk/src/connections/network/network.cpp:420:45: error: template argument 1 is invalid
std::lock_guard<std::recursive_mutex> guard(m_mutex);
^
/home/sebmenet/Sebastien_Menet/aditof_sdk/sdk/src/connections/network/network.cpp:420:53: error: ‘m_mutex’ was not declared in this scope
std::lock_guard<std::recursive_mutex> guard(m_mutex);
^~~~~~~
/home/sebmenet/Sebastien_Menet/aditof_sdk/sdk/src/connections/network/network.cpp:426:38: warning: ‘int google::protobuf::MessageLite::ByteSize() const’ is deprecated: Please use ByteSizeLong() instead [-Wdeprecated-declarations]
int siz = send_buff.ByteSize();

[ 2%] Building CXX object sdk/CMakeFiles/aditof.dir/src/connections/network/network.cpp.o
sdk/CMakeFiles/aditof.dir/build.make:349: recipe for target 'sdk/CMakeFiles/aditof.dir/src/connections/network/network.cpp.o' failed
CMakeFiles/Makefile2:226: recipe for target 'sdk/CMakeFiles/aditof.dir/all' failed
Makefile:135: recipe for target 'all' failed