Hello,
I am working on a project to do real time image recognition using the AD-96ToF1-EBZ time of flight sensor from Analog Devices on the DragonBoard 410c embedded platform, but want to make sure I have the latest SD card image flashed for booting the Linux OS. When I first received the sensor in the mail, The SD card had a Linux OS on it with a sensor demo that I was able to try and verify the sensor was functioning properly. However, I was unable to connect to the internet even when using the "$ nmtui" command because I could not find my home network in the network manager list. My wifi is not 5 GHz, it is 2.4 GHz so that should not be the issue here. I tried flashing what the GitHub claimed was the latest SD card image for the dragonboard 410c, but after flashing it, I found that it was an android OS but I could not find the demos anymore. I was able to connect to the internet but I was under the impression I would have a Linux OS boot with the demo. I would like the latest Linux OS with the demo and internet capabilities if possible. Any help is sincerely appreciated!
Added product category
[edited by: GenevaCooper at 2:39 PM (GMT -5) on 3 Jan 2023]