Post Go back to editing

Could you please let me know the product number and serial number of your Xavier NX which worked well with AD-FXTOF1-EBZ ?

Hello,

Our customer have two Xavier NXs. They tested them with AD-FXTOF1-EBZ.

One Xavier NX worked well with AD-FXTOF1-EBZ, but the other did not work properly. Please refer to the log files.

[sudo] password for analog: 
I1215 13:54:20.140313  8909 sensor_enumerator_xaviernx.cpp:49] Looking for devices on the target: Xavier NX
I1215 13:54:20.142510  8909 camera_fxtof1.cpp:127] Initializing camera
I1215 13:54:20.142577  8909 addi9036_sensor.cpp:140] Opening device
I1215 13:54:20.142643  8909 addi9036_sensor.cpp:158] Looking for the following cards:
I1215 13:54:20.142683  8909 addi9036_sensor.cpp:160] vi-output, addi9036 9-0064
I1215 13:54:20.142730  8909 addi9036_sensor.cpp:160] vi-output, addi9036 10-0064
E1215 13:54:20.146088  8909 tmp10x_sensor.cpp:60] Temp sensor open error
I1215 13:54:20.385713  8909 camera_fxtof1.cpp:178] Camera initialized
I1215 13:54:20.388234  8909 addi9036_sensor.cpp:257] Starting device 0
I1215 13:54:20.397008  8909 addi9036_sensor.cpp:257] Starting device 1
I1215 13:54:20.463418  8909 camera_fxtof1.cpp:209] Chosen mode: near
I1215 13:54:20.463584  8909 camera_fxtof1.cpp:222] Camera range for mode: near is: 250 mm and 800 mm
I1215 13:54:20.463744  8909 camera_fxtof1.cpp:233] Found firmware for mode: near
I1215 13:54:20.463816  8909 camera_fxtof1.cpp:236] Firmware size: 14404 bytes
I1215 13:54:21.864408  8909 calibration_fxtof1.cpp:278] Camera intrinsic parameters:
    fx: 376.125
    fy: 375.899
    cx: 321.253
    cy: 226.786

[sudo] password for analog: 
I1122 11:38:57.054841  7741 sensor_enumerator_xaviernx.cpp:49] Looking for devices on the target: Xavier NX
I1122 11:38:57.056882  7741 camera_fxtof1.cpp:127] Initializing camera
I1122 11:38:57.056962  7741 addi9036_sensor.cpp:140] Opening device
I1122 11:38:57.057037  7741 addi9036_sensor.cpp:158] Looking for the following cards:
I1122 11:38:57.057078  7741 addi9036_sensor.cpp:160] vi-output, addi9036 9-0064
I1122 11:38:57.057112  7741 addi9036_sensor.cpp:160] vi-output, addi9036 10-0064
I1122 11:38:57.304137  7741 camera_fxtof1.cpp:178] Camera initialized
I1122 11:38:57.306660  7741 addi9036_sensor.cpp:257] Starting device 0
W1122 11:38:57.312093  7741 addi9036_sensor.cpp:276] VIDIOC_STREAMON error errno: 22 error: Invalid argument
I1122 11:38:57.381633  7741 camera_fxtof1.cpp:209] Chosen mode: near
I1122 11:38:57.381767  7741 camera_fxtof1.cpp:222] Camera range for mode: near is: 250 mm and 800 mm
I1122 11:38:57.381889  7741 camera_fxtof1.cpp:233] Found firmware for mode: near
I1122 11:38:57.381986  7741 camera_fxtof1.cpp:236] Firmware size: 14404 bytes
I1122 11:39:00.381466  7741 calibration_fxtof1.cpp:278] Camera intrinsic parameters:
    fx: 376.125
    fy: 375.899
    cx: 321.253
    cy: 226.786
W1122 11:39:02.947105  7787 addi9036_sensor.cpp:868] VIDIOC_DQBUF error errno: 22 error: Invalid argument
W1122 11:39:02.947361  7787 camera_fxtof1.cpp:371] Failed to get frame from device

They also tested them with Raspberry Pi Camera module V2 and confirmed the Xavier NXs worked well.

https://akizukidenshi.com/catalog/g/gM-10518/

 

[Questions]

[1] Could you please let me know the product number and serial number of your Xavier NX which worked well with AD-FXTOF1-EBZ ?

     You can confirm them by “sudo i2cdump -f -y 0 0x50” command.

     The customer confirmed their Xavier NX boards have same information as below.

  Major Version Number0x01

  Minor Version Number0x00

  Product Part Number699-13668-0000-200 H.0

[2] Are there any restrictions about Xavier NX when using with AD-FXTOF1-EBZ ? 

Best regards,

H.Kashima



Modified Xaiver to Xavier.
[edited by: HYKS at 9:50 AM (GMT -5) on 16 Dec 2021]
Parents Reply Children
No Data