Post Go back to editing

failed to read firmware from eeprom

Thread Summary

The user encountered an EEPROM firmware read error when running aditof-demo.sh on a Dragonboard 410c with AD96 TOF board. The issue was resolved by rewriting the EEPROM with a new image from the aditof_sdk repository and reflashing the SD card with a new image. The user also faced USB communication issues when connecting the Dragonboard to a Linux PC, which were mitigated by ensuring the uvc-gadget application correctly advertised the EEPROM storage and using a different USB cable.
AI Generated Content

I am using the AD96 TOF board with Dragonboard 410c, I have connected a display and mouse+keyboard to the dragon board. I see the error Failed to read frirmware from eeprom in the terminal when I try to run the aditof-demo.sh

I have updated the sdk on the sd card following the build instructions here https://github.com/analogdevicesinc/aditof_sdk/blob/master/doc/dragonboard410c/build_instructions.md

Although I was able to run the aditof-demo.sh initially on the dragonboard, I then attempted to connect the dragon board over USB to PC and run the aditof-demo on a linux PC where the eeprom firmware error first showed up, Reverting to the dragon board setup I see the same issue while trying to run the aditof-demo on the dragonboard now. 

Please help me with any leads on how I can identify what is missing at my end which could be creating this issue?, I have tried running the eeprom tool which returns segmentation fault.

  

Parents
  • Can you run aditof-demo again on Dragonboard 410c and copy the entire output printed by the demo and paste it here?

  • linaro@linaro-alip:~/Desktop$ ./aditof-demo.sh
    Opening media device /dev/media1
    Enumerating entities
    looking up device: 81:4
    looking up device: 81:5
    looking up device: 81:6
    looking up device: 81:7
    looking up device: 81:8
    looking up device: 81:9
    looking up device: 81:10
    looking up device: 81:0
    looking up device: 81:11
    looking up device: 81:1
    looking up device: 81:12
    looking up device: 81:2
    looking up device: 81:13
    looking up device: 81:3
    looking up device: 81:14
    Found 15 entities
    Enumerating pads and links
    Setting up link 4:1 -> 7:0 [1]
    Opening media device /dev/media1
    Setting up link 7:1 -> 13:0 [1]
    Opening media device /dev/media1
    Setting up link 13:1 -> 19:0 [1]
    Opening media device /dev/media1
    Opening media device /dev/media1
    Enumerating entities
    looking up device: 81:4
    looking up device: 81:5
    looking up device: 81:6
    looking up device: 81:7
    looking up device: 81:8
    looking up device: 81:9
    looking up device: 81:10
    looking up device: 81:0
    looking up device: 81:11
    looking up device: 81:1
    looking up device: 81:12
    looking up device: 81:2
    looking up device: 81:13
    looking up device: 81:3
    looking up device: 81:14
    Found 15 entities
    Enumerating pads and links
    Setting up format SBGGR12_1X12 640x960 on pad addi903x 1-0064/0
    Format set: SBGGR12_1X12 640x960
    Setting up format SBGGR12_1X12 640x960 on pad msm_csiphy1/0
    Format set: SBGGR12_1X12 640x960
    Setting up format SBGGR12_1X12 640x960 on pad msm_csid0/0
    Format set: SBGGR12_1X12 640x960
    Setting up format SBGGR12_1X12 640x960 on pad msm_ispif0/0
    Format set: SBGGR12_1X12 640x960
    Setting up format SBGGR12_1X12 640x960 on pad msm_vfe0_rdi0/0
    Format set: SBGGR12_1X12 640x960
    I0120 18:21:59.417076 4198 sensor_enumerator_dragonboard.cpp:156] Looking for sensors on the target
    I0120 18:21:59.418447 4198 sensor_enumerator_dragonboard.cpp:176] Looking at: /dev/media1 for an eligible TOF camera
    I0120 18:21:59.491503 4198 sensor_enumerator_dragonboard.cpp:190] Considering: /dev/media1 an eligible TOF camera
    I0120 18:21:59.491757 4198 sensor_enumerator_dragonboard.cpp:176] Looking at: /dev/media0 for an eligible TOF camera
    I0120 18:21:59.526357 4198 camera_96tof1.cpp:144] Initializing camera
    I0120 18:21:59.526518 4198 addi9036_sensor.cpp:139] Opening device
    I0120 18:21:59.526662 4198 addi9036_sensor.cpp:157] Looking for the following cards:
    I0120 18:21:59.526736 4198 addi9036_sensor.cpp:159] Qualcomm Camera Subsystem
    I0120 18:22:00.352267 4198 calibration_96tof1.cpp:164] EEPROM calibration data size 64940 bytes
    I0120 18:22:09.803375 4198 camera_96tof1.cpp:200] Camera initialized
    W0120 18:22:09.803656 4198 calibration_96tof1.cpp:346] No intrinsics found in the device memory for key 5.000000
    W0120 18:22:09.804540 4198 calibration_96tof1.cpp:346] No intrinsics found in the device memory for key 6.000000
    I0120 18:22:09.806912 4198 addi9036_sensor.cpp:254] Starting device 0
    I0120 18:22:09.863178 4198 camera_96tof1.cpp:231] Chosen mode: near
    I0120 18:22:09.863487 4198 camera_96tof1.cpp:273] Camera range for mode: near is: 250 mm and 800 mm
    W0120 18:22:09.863664 4198 camera_96tof1.cpp:280] Failed to read firmware from eeprom
    I0120 18:22:13.806234 4198 addi9036_sensor.cpp:296] Stopping device

  •  , do any of the command line outputs point to any leads on why I could be facing this issue? is there a way to check if there is an issue with the eeprom on the board itself or its just a software issue?

    My concern is that the demo was running fine when I first connected and booted the 410c board, only after I tried to connect to a linux PC I have run into this issue. Let me know if I could share any other detail that could help debug this issue.

Reply
  •  , do any of the command line outputs point to any leads on why I could be facing this issue? is there a way to check if there is an issue with the eeprom on the board itself or its just a software issue?

    My concern is that the demo was running fine when I first connected and booted the 410c board, only after I tried to connect to a linux PC I have run into this issue. Let me know if I could share any other detail that could help debug this issue.

Children