The example in https://github.com/analogdevicesinc/adi_3dtof_image_stitching shows simultaneous operation of 4 sensors observing the same scene.
It is not clear however if the sensors are hardware synchronised to avoid potential interference between each other.
Can you please clarify:
1) How is interference due to light from other cameras sources handled ?
2) Is there any hardware multi-device synchronisation mode to avoid the above? If so, can you provide more details on that ?
3) Is there a maximum number of sensors that can be used to observe the same scene ?