Post Go back to editing

After I ran data_collect, the EVAL-ADTF3175D-NXZ did not work any more.

Category: Software
Product Number: EVAL-ADTF3175D-NXZ
Software Version: TOF_Evaluation_ADTF3175D-Rel3.2.0

Hello, 

After I ran following data_collect on Windows 10 Pro, the EVAL-ADTF3175D-NXZ does not work any more.

--------


c:\Analog Devices\TOF_Evaluation_ADTF3175D-Rel3.2.0\bin>data_collect.exe --ip 10.42.0.1 --fw fwUpdate_3.2.2.bin tof-viewer_config.json
I20230607 16:01:35.414691 32108 main.cpp:281] SDK version: 3.2.0 | branch: master | commit: a5aba864
I20230607 16:01:35.424692 32108 main.cpp:423] Output folder: ./
I20230607 16:01:35.425691 32108 main.cpp:424] Mode: 10
I20230607 16:01:35.425691 32108 main.cpp:425] Number of frames: 1
I20230607 16:01:35.425691 32108 main.cpp:426] Json file: tof-viewer_config.json
I20230607 16:01:35.426692 32108 main.cpp:427] Frame type is: raw
I20230607 16:01:35.426692 32108 main.cpp:428] Warm Up Time is: 0 seconds
I20230607 16:01:35.427690 32108 main.cpp:431] Ip address is: 10.42.0.1
I20230607 16:01:35.427690 32108 main.cpp:435] Firmware file is is: fwUpdate_3.2.2.bin
I20230607 16:01:35.428690 32108 system_impl.cpp:130] SDK built with websockets version:3.1.0
I20230607 16:01:35.431700 32108 network_sensor_enumerator.cpp:53] Looking for sensors over network
[2023/06/07 16:01:35:4376] NOTICE: Creating Vhost 'default' (serving disabled), 1 protocols, IPv6 off
Conn established
Connection Closed
I20230607 16:01:35.514691 32108 camera_itof.cpp:142] Initializing camera
[2023/06/07 16:01:35:5206] NOTICE: Creating Vhost 'default' (serving disabled), 1 protocols, IPv6 off
Conn established
I20230607 16:01:40.674693 32108 mode_info.cpp:149] Using old modes table.
I20230607 16:01:40.748689 32108 camera_itof.cpp:245] Current adsd3500 firmware version is: 4.2.1.0
I20230607 16:01:40.749689 32108 camera_itof.cpp:248] Current adsd3500 firmware git hash is: a59afad6d6c8e7fb153a2db8cd8840359f17195a
I20230607 16:01:40.751693 32108 camera_itof.cpp:1607] Found Depth ini file: ../config/RawToDepthAdsd3500_lrqmp.ini
I20230607 16:01:40.751693 32108 camera_itof.cpp:1607] Found Depth ini file: ../config/RawToDepthAdsd3500_lrmp.ini
I20230607 16:01:40.752691 32108 camera_itof.cpp:1607] Found Depth ini file: ../config/RawToDepthAdsd3500_srqmp.ini
I20230607 16:01:40.752691 32108 camera_itof.cpp:1607] Found Depth ini file: ../config/RawToDepthAdsd3500_srmp.ini
I20230607 16:01:40.752691 32108 camera_itof.cpp:1618] Current Depth ini file is: ../config/RawToDepthAdsd3500_lrmp.ini
I20230607 16:01:40.758689 32108 camera_itof.cpp:343] Camera FPS set from Json file at: 10
I20230607 16:01:40.762689 32108 camera_itof.cpp:355] Camera initialized
I20230607 16:01:40.763691 32108 main.cpp:474] SD card image version: microsd-a5aba864.img
I20230607 16:01:40.763691 32108 main.cpp:475] Kernel version: lf-5.10.72-2.2.0
I20230607 16:01:40.763691 32108 main.cpp:476] U-Boot version: imx_v2020.04_5.4.70_2.3.0
I20230607 16:01:40.767693 32108 camera_itof.cpp:1268] The readback chip ID is: 22833
I20230607 16:01:41.077692 32108 camera_itof.cpp:1338] Succesfully sent 0 out of 360 packets
I20230607 16:01:45.008693 32108 camera_itof.cpp:1338] Succesfully sent 25 out of 360 packets
I20230607 16:01:48.476694 32108 camera_itof.cpp:1338] Succesfully sent 50 out of 360 packets
I20230607 16:01:52.862694 32108 camera_itof.cpp:1338] Succesfully sent 75 out of 360 packets
I20230607 16:01:56.127691 32108 camera_itof.cpp:1338] Succesfully sent 100 out of 360 packets
I20230607 16:01:59.387729 32108 camera_itof.cpp:1338] Succesfully sent 125 out of 360 packets
I20230607 16:02:03.801396 32108 camera_itof.cpp:1338] Succesfully sent 150 out of 360 packets
I20230607 16:02:07.429396 32108 camera_itof.cpp:1338] Succesfully sent 175 out of 360 packets
I20230607 16:02:10.704399 32108 camera_itof.cpp:1338] Succesfully sent 200 out of 360 packets
I20230607 16:02:14.439396 32108 camera_itof.cpp:1338] Succesfully sent 225 out of 360 packets
I20230607 16:02:19.952394 32108 camera_itof.cpp:1338] Succesfully sent 250 out of 360 packets
I20230607 16:02:24.788396 32108 camera_itof.cpp:1338] Succesfully sent 275 out of 360 packets
I20230607 16:02:30.510401 32108 camera_itof.cpp:1338] Succesfully sent 300 out of 360 packets
I20230607 16:02:35.375394 32108 camera_itof.cpp:1338] Succesfully sent 325 out of 360 packets
I20230607 16:02:38.659402 32108 camera_itof.cpp:1338] Succesfully sent 350 out of 360 packets
I20230607 16:02:39.942399 32108 camera_itof.cpp:1353] Adsd3500 firmware updated succesfully!
I20230607 16:02:39.943400 32108 main.cpp:484] Please reboot the board!
Connection Closed

c:\Analog Devices\TOF_Evaluation_ADTF3175D-Rel3.2.0\bin>

----------------------------------------------------------------------

[Test 1]

When I ran ADIToFGUI.exe in TOF_Evaluation_ADTF3175D-Rel3.2.0, 

I got the error messages as below.

"Failed to read dealias parameters for adsd3500!

 Could not initialize camera! "

[Test 2]

When I tried data_collect to write Fw_updata_4.1.5.bin, I also got the same error messages.

It seems that adsd3500 did not work properly.

Could you kindly let me know how to recover the EVAL-ADTF3175D-NXZ ?

Best regards,

H.Kashima

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.