Q
The datasheet states on the frontpage that avdd can be 5v while dvdd is 3V.
Absolute max. Ratings state that avdd to dvdd should be -0.3V to 0.3v. Which is
true
A
There is an error in the absolute maximum ratings, the -0.3V to 0.3v
restriction on AVDD to DVDD should not be there and will be removed in next
revision of the datasheet.