This webinar will introduce remote-controlled edge nodes and how they promise to simplify the automotive network architecture and expedite the integration...
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
      1. Quote of the week: "Knowledge is knowing a tomato is a fruit. Wisdom is not putting it in a fruit salad" - unknown Sources: commons.wikimedia...

    View All

    What's Brewing

      Quiz! Why a Hybrid Approach Works Blog and Test Your Knowledge

      Quiz! Understand ISO 26262 Compliance Test your knowledge with our quick quiz , based on the blog " Safety in Layers: Why a Hybrid Approach Works ...
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
    The Limitation of Heat Dissipation IO-Link is used across many branches of factory automation, and in these applications, areas of the factory floor...

     

    GMSL Debugging: Getting a Lock

    Imagine a scenario where you have a brand-new board design or are excited to try out some evaluation kits only to find out that the two devices can’t talk...
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
Direct Digital Synthesis (DDS)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Direct Digital Synthesis (DDS)
Direct Digital Synthesis (DDS)
Documents AD9851: Best value for Rset
  • Forums
  • FAQs/Docs
  • Members
  • Tags
  • More
  • Cancel
  • Documents
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • +AD5934: FAQ
  • +AD9152: FAQ
  • +AD9830: FAQ
  • +AD9832: FAQ
  • +AD9833: FAQ
  • +AD9834: FAQ
  • +AD9835: FAQ
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9840: FAQ
  • +AD9840A: FAQ
  • +AD9845A: FAQ
  • +AD9850: FAQ
  • -AD9851: FAQ
    • AD9851: Best value for Rset
    • AD9851: frequency senthesis
    • AD9851: RESET input
  • +AD9852: FAQ
  • +AD9854: FAQ
  • +AD9854ASQ: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9858: FAQ
  • +AD9859: FAQ
  • +AD9910: FAQ
  • +AD9912: FAQ
  • +AD9913: FAQ
  • +AD9914: FAQ
  • +AD9915: FAQ
  • +AD9945: FAQ
  • +AD9951: FAQ
  • +AD9952: FAQ
  • +AD9953: FAQ
  • +AD9954: FAQ
  • +AD9956: FAQ
  • +AD9957: FAQ
  • +AD9958: FAQ
  • +AD9959: FAQ
  • +DDS: FAQ
  • +Digital Ground (DGND): FAQ
  • +Evaluation Software: FAQ
  • +Frequency Ramp: FAQ
  • +I/O_UPDATE: FAQ
  • +Maximum Clock Rate: FAQ
  • +PLL: FAQ
  • +Programmable Modulus: FAQ
  • +SFDR: FAQ
  • +Thermally Enhanced Packages: FAQ

AD9851: Best value for Rset

Q 

In your datasheet you show an AD9851 with both outputs connected to a
Minicircuits T1-1T transformer, the primary center-tap is grounded.

What value of Rset should be used in this configuration?

 

A 

Rset sets the full scale output current of AD9851. Output current can be set
from 5mA to 20mA with optimal performance at 10mA.

The value of Rset is related to full scale output current IOUT by Rset =
39.93/IOUT

This means approximately
2k for 20mA
4k for 10mA
8k for 5mA

A T1-1T transformer (1:1 turns ratio) can handle up to 250mW input power and
30mA DC current. The maximum output current of the AD9851 is 20mA, and with 50
Ohm termination this gives 20mW of input power. So the transformer does not
impose a limit on the output current of the DAC.

Referring to figure 9 in the AD9851 datasheet, the only case where trouble
could arise would be if the filter had a very high input impedance. The DAC has
a compliance of +1.5V maximum. If the impedance of the filter were higher than
60 Ohms OVER THE TRANSFORMER FREQUENCY RANGE 80kHz to 200MHz then the DAC
compliance range might be exceeded with a current setting of 20mA. The benefit
of the transformer coupling is that it blocks the DC component of the output
signal, so that the filter can have very high input impedance at DC without
exceeding the compliance range of the AD9851 output.

So the answer to your question depends on the impedance of the filter (compare
with figure 9) and the frequency range of the transformer. IF the filter has
moderate input impedance over the transformer bandwidth then the optimum
setting of 10mA = 3.92kOhms should be fine. Otherwise you can either reduce the
full scale output current or add a shunt resistor before the filter to reduce
the output impedance (but you lose some signal ampitude in the process)

Tags: ad9851