Join us for an exciting webinar where we will unveil and demonstrate our new bulk ordering and bulk quoting tools! Discover how you can streamline your...
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
      1. First, the quote of the week: " The best measure of a man's honesty isn't his income tax return. It's the zero adjust on his bathroom scale " - Unknown...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: White Coats and Multi-Coloured Pens Ready to put...
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
    How can we meet the growing power requirements of the future? 5G network deployments necessitate high-efficiency power conversion solutions capable of...

     

    Freedom from Interference: Control of Mixed ASIL Criticalities

    Interference, within the context of Functional Safety, refers to a situation in which a failure in a component of a system may propagate to other components...

    Latest Blogs

    • High-Tech Pro and Crafty Creator: Meet Iulia, Our Inspiring Super User!
    • Apples and Oranges: A Comparative Study of DCM and CCM: Part 6 of 6
    • Understanding AXI-Stream Interfaces for DSP Data Pipelines
    • Importing Op Amp Models in LTspice: When All Else Fails, Customize the Symbol: Part 3 of 3
    • Inside the Bits: Digging Deeper with Part-Specific Register Examples
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
Direct Digital Synthesis (DDS)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Direct Digital Synthesis (DDS)
Direct Digital Synthesis (DDS)
Documents AD9856: Pin connection
  • Forums
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • +AD5934: FAQ
  • +AD9152: FAQ
  • +AD9830: FAQ
  • +AD9832: FAQ
  • +AD9833: FAQ
  • +AD9834: FAQ
  • +AD9835: FAQ
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9840: FAQ
  • +AD9840A: FAQ
  • +AD9845A: FAQ
  • +AD9850: FAQ
  • +AD9851: FAQ
  • +AD9852: FAQ
  • +AD9854: FAQ
  • +AD9854ASQ: FAQ
  • -AD9856: FAQ
    • AD9856: Pin connection
    • Can you send me the AD9856 filter coefficients?
  • +AD9857: FAQ
  • +AD9858: FAQ
  • +AD9859: FAQ
  • +AD9910: FAQ
  • +AD9912: FAQ
  • +AD9913: FAQ
  • +AD9914: FAQ
  • +AD9915: FAQ
  • +AD9945: FAQ
  • +AD9951: FAQ
  • +AD9952: FAQ
  • +AD9953: FAQ
  • +AD9954: FAQ
  • +AD9956: FAQ
  • +AD9957: FAQ
  • +AD9958: FAQ
  • +AD9959: FAQ
  • +DDS: FAQ
  • +Digital Ground (DGND): FAQ
  • +Evaluation Software: FAQ
  • +Frequency Ramp: FAQ
  • +I/O_UPDATE: FAQ
  • +Maximum Clock Rate: FAQ
  • +PLL: FAQ
  • +Programmable Modulus: FAQ
  • +SFDR: FAQ
  • +Thermally Enhanced Packages: FAQ

AD9856: Pin connection

Q 

I am investigating problems on a PCB containing an AD9856. The SDIO pin
is driven from a 244 buffer however there appears to be contention on
this pin.

I am not sure whether some pins on the device are connected correctly.
The PLL SUPPLY pin is connected to PLL GND as we are not using the PLL.
Is this OK?

Also the SYNC I/O pin is connected to ground via a 10K resistor. Should
we be using this pin to ensure integrity of the serial control link?

 

A 

Even if you are not using the Reference clock you should still connect Vpll to
3V and disable the reference clock multiplier in the register 01H.

The serial interface of the AD9856 is synchronous and it is essential that the
part sees exactly the right number of clock edges  during each communications
cycle. Reading or writing one too many or one too few bytes during a
communications cycle will cause synchronisation of the interface to be lost.
Similarly any spurious glitches on the SCLK line could be interpreted as clock
edge and will throw the serial port out of sync.

If multiple sources are able to drive the SCLK pin or if poor grounding and
board layout allow coupling of some other signal onto the SCLK line, the
interface could be getting out of sync regularly. The interface can be reset to
it's default state of expecting an instruction byte by proving a high going
pulse on the SYNC IO pin. Controlling the SYNC IO pin is a  useful way out when
synchronisation is lost but you'll need to look carefully at your board and
determine what is causing the interface to get lost in the first place.

Tags: ad9856
  • Share
  • History
  • More