Locale Icon
English
  • Forums

    Popular Forums

    • LTspice
    • RF and Microwave
    • Video
    • Power Management
    • Precision ADCs
    • FPGA Reference Designs
    • Linux Software Drivers

    Product Forums

    • Amplifiers
    • Microcontrollers
    • Clock and Timing
    • Data Converters
    • Direct Digital Synthesis (DDS)
    • Energy Monitoring and Metering
    • Interface and Isolation
    • MEMS Inertial Sensors
    • Power Management
    • Processors and DSP
    • Switches/Multiplexers
    • Temperature Sensors
    • Voltage References
    View All

    Application Forums

    • A2B
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
    • Design Tools and Calculators
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
    The Burning Question: How can ADI Solutions Ensure Rechargeable Device Batteries are Genuine?

    On the global stage, products and equipment using rechargeable batteries continue to proliferate exponentially, expecting to reach a staggering $170B market...
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
    • Maximize Your Power Regulator: Key Considerations for Thermal Performance
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quizzes AQQ294 about a digital phase splitter design

      1. Quote of the month: "I've learned that people will forget what you said, people will forget what you did, but people will never forget how you made...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Let's Take a Field-Bus Trip Your field-bus engines...
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
    Balancing Enhanced Radar Resolution with FPGA-Based Pulse Compression

    Radar and sonar systems must balance range resolution with the energy required for reliable detection. Pulse compression resolves this by sending a long...

     

    ​​ISO 26262 Essentials: Ensuring Confidence in Your Software Tools ​

    By Ashish Iskande What is Tool Qualification and Why is it Important? In safety-critical automotive development, tools act as silent partners but can...

    Latest Blogs

    • Step-by-Step: Implementing a Complete DSP Chain for Signal Analysis
    • Galvanic Isolation in SMPS: Ensuring Safety and Protection: Part 1 of 4
    • Mature, Not Old! The Longevity of 4 – 20 mA
    • Turning up the Noise: .NOISE Simulations in LTspice: Part 1 of 3
    • The ABCs of SerDes
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
Direct Digital Synthesis (DDS)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Direct Digital Synthesis (DDS)
Direct Digital Synthesis (DDS)
Documents AD9910: output circuit clarification
  • Forums
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • +AD5934: FAQ
  • +AD9152: FAQ
  • +AD9830: FAQ
  • +AD9832: FAQ
  • +AD9833: FAQ
  • +AD9834: FAQ
  • +AD9835: FAQ
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9840: FAQ
  • +AD9840A: FAQ
  • +AD9845A: FAQ
  • +AD9850: FAQ
  • +AD9851: FAQ
  • +AD9852: FAQ
  • +AD9854: FAQ
  • +AD9854ASQ: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9858: FAQ
  • +AD9859: FAQ
  • -AD9910: FAQ
    • AD9910 and AD9912: Residual Phase Noise Definition and Measurement
    • AD9910 Evaluation board driver for Win7
    • AD9910 frequency update rate
    • AD9910: EVB R43 resistor value
    • AD9910: output circuit clarification
    • AD9910: output filter design
    • AD9910: Programming through SPI-Interface
    • AD9910: REFCLK termination
    • AD9910: REFCLK termination 2
    • AD9910EVB_Filter Question
    • AD9910_Multichip SYNCHRONIZATION.
    • AD9910_output amplitude flatness over frequency
    • AD9910_phase noise
    • AD9910_phase truncation bits
    • DDS_harmonic or image phase adjustment
  • +AD9912: FAQ
  • +AD9913: FAQ
  • +AD9914: FAQ
  • +AD9915: FAQ
  • +AD9945: FAQ
  • +AD9951: FAQ
  • +AD9952: FAQ
  • +AD9953: FAQ
  • +AD9954: FAQ
  • +AD9956: FAQ
  • +AD9957: FAQ
  • +AD9958: FAQ
  • +AD9959: FAQ
  • +DDS: FAQ
  • +Digital Ground (DGND): FAQ
  • +Evaluation Software: FAQ
  • +Frequency Ramp: FAQ
  • +I/O_UPDATE: FAQ
  • +Maximum Clock Rate: FAQ
  • +PLL: FAQ
  • +Programmable Modulus: FAQ
  • +SFDR: FAQ
  • +Thermally Enhanced Packages: FAQ

AD9910: output circuit clarification

Q 

About the output circuit of the AD9910 eval board , after a deeper analysis,
there are several inconsistencies and items that you may need to be aware of
and I thought you'd find this discussion interesting and useful. I've
summarized in the attached file.

 

A 

1) 75 ohm transformer in a 50 ohm circuit: Here's the word from
Andrew@minicircuits.com: When you operate a 75 Ohm transformer in a 50 Ohm
system you should expect the operational bandwidth to be slightly shifted in
frequency. So if you are using the transformer in the specified central
frequency region, there should be no practical difference. We picked this part
because of its wide bandwidth (800MHz). Because it is not operated in a 75 ohm
system, we expect this BW to decrease somewhat (according to Mini-Circuits),
but it will still be far larger than all the Mini-Circuits 50 ohm transformers
we've found.

2) If you look at the transformer's datasheet (attached here), the primary has
no center-tap (i.e., pin 5 is not used) while the secondary does. Since we need
the DDS outputs to be biased, we operate the transformer "backwards" so that
the center-tap is on the DDS side of the circuit to provide this bias. That is,
we connect the transformer such that it's secondary windings act as the primary
and vica-versa. Because this is a 1:1 transformer, this can be done without any
strange effects. We grounded pin 5 because it shorts out a potential parasitic
signal input path and was easy to do.

3) With both sides of the DDS terminated in 50 ohms, the equivalent resistance
seen at the transformer input is 100 ohms. Since this is a 1:1 transformer,
this resistance is reflected to the output of the transformer. The
reconstruction filter sees a 100 ohm source resistance. However, the design of
filter assumed a 50 ohm source and load. Because of this, the frequency
response of the filter will not be what was intended. However, if you look at
the filter's simulated response (see attached Spice simulation), it hasn't
changed much. Compared to a 50 ohm source, the 100 ohm source allows a higher
output level (because the DDS is driving a higher impedance) but also has
slightly more ripple. Note that transformer bandwidth effects have not been
included nor has the ultimate attenuation limitations of PCB stray signal paths
& non-ideal grounding.

Attachments:
AD9910_outputcircuitclarification.zip
Tags: ad9910
  • Share
  • History
  • More
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
©2025 Analog Devices, Inc. All Rights Reserved
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
©2025 Analog Devices, Inc. All Rights Reserved