Join us for an in-depth webinar where we dive into the world of EMC testing applied to ADI’s digital isolators. We''ll walk through the test setups, standards...
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
      KCC's Quizzes AQQ294 about a digital phase splitter design

      1. Quote of the month: "I've learned that people will forget what you said, people will forget what you did, but people will never forget how you made...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: White Coats and Multi-Coloured Pens Ready to put...
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
    By Christopher Nunes What happens when your system needs to talk across noisy or high-voltage boundaries? Isolation steps in. In a previous blog post...

     

    Understanding Safe Failure Fraction: Can There Be Multiple Values?

    I discuss various aspects of the SFF (safe failure fraction) —whether it applies to an integrated circuit —and whether an integrated circuit can have more...
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
Direct Digital Synthesis (DDS)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Direct Digital Synthesis (DDS)
Direct Digital Synthesis (DDS)
Documents AD9910 frequency update rate
  • Forums
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • +AD5934: FAQ
  • +AD9152: FAQ
  • +AD9830: FAQ
  • +AD9832: FAQ
  • +AD9833: FAQ
  • +AD9834: FAQ
  • +AD9835: FAQ
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9840: FAQ
  • +AD9840A: FAQ
  • +AD9845A: FAQ
  • +AD9850: FAQ
  • +AD9851: FAQ
  • +AD9852: FAQ
  • +AD9854: FAQ
  • +AD9854ASQ: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9858: FAQ
  • +AD9859: FAQ
  • -AD9910: FAQ
    • AD9910 and AD9912: Residual Phase Noise Definition and Measurement
    • AD9910 Evaluation board driver for Win7
    • AD9910 frequency update rate
    • AD9910: EVB R43 resistor value
    • AD9910: output circuit clarification
    • AD9910: output filter design
    • AD9910: Programming through SPI-Interface
    • AD9910: REFCLK termination
    • AD9910: REFCLK termination 2
    • AD9910EVB_Filter Question
    • AD9910_Multichip SYNCHRONIZATION.
    • AD9910_output amplitude flatness over frequency
    • AD9910_phase noise
    • AD9910_phase truncation bits
    • DDS_harmonic or image phase adjustment
  • +AD9912: FAQ
  • +AD9913: FAQ
  • +AD9914: FAQ
  • +AD9915: FAQ
  • +AD9945: FAQ
  • +AD9951: FAQ
  • +AD9952: FAQ
  • +AD9953: FAQ
  • +AD9954: FAQ
  • +AD9956: FAQ
  • +AD9957: FAQ
  • +AD9958: FAQ
  • +AD9959: FAQ
  • +DDS: FAQ
  • +Digital Ground (DGND): FAQ
  • +Evaluation Software: FAQ
  • +Frequency Ramp: FAQ
  • +I/O_UPDATE: FAQ
  • +Maximum Clock Rate: FAQ
  • +PLL: FAQ
  • +Programmable Modulus: FAQ
  • +SFDR: FAQ
  • +Thermally Enhanced Packages: FAQ

AD9910 frequency update rate

Q 

I am hoping to use one of your DDS devices as a chirp generator in a radar
system I am currently developing.

1) Am I correct in assuming that the AD9910 will allow me to generate a linear
frequency ramp with a frequency step time interval / update rate of 4nS ?

2) Does the AD9910 offer the fastest frequency update rate in your DDS range or
is there a faster device available ?

3) Do you have a road map which details how the frequency update rates of your
DDS devices are likely to increase in the future ?

 

A 

1) Am I correct in assuming that the AD9910 will allow me to generate a linear
frequency ramp with a frequency step time interval / update rate of 4nS ?
->Yes. The fastest frequency step time interval setting is equal to the
SYNC_CLK rate. The SYNC_CLK rate = system clock / 4. So, if the system clock is
1GHz then the period of the SYNC_CLLK is 4ns.

2) Does the AD9910 offer the fastest frequency update rate in your DDS range or
is there a faster device available ?
->If the DRG is the source of the frequency ramp, then yes the AD9910 provides
the fastest frequency step time interval setting.
However, if the frequency tuning word is provided externally on the fly for
whatever reason, the AD9915 has a full 32-bit BUS which provides a faster way
to update the 32-BIT FTW faster. In that case,
The update rate is also the SYNC_CLK rate. In that part, the SYNC_CLK is system
clock/ 16. So, if the system clock is 2.5GHz then the period of the SYNC_CLLK
is  approximately 7ns. The AD9910 cannot update the full 32-bit FTW faster than
that.

3) Do you have a road map which details how the frequency update rates of your
DDS devices are likely to increase in the future ?
->TBD

Tags: ad9910
  • Share
  • History
  • More