Hi
For ad9958 could perform both linear frequency sweep and phase modulation simultaneously for both channels?
if yes, could you give me some notes who can assign profile and SDIO_x pins to do this?
regards
AD9958
Recommended for New Designs
The AD9958 consists of two DDS cores that provide independent
frequency, phase, and amplitude control on each channel.
This flexibility can be used to...
Datasheet
AD9958 on Analog.com
Hi
For ad9958 could perform both linear frequency sweep and phase modulation simultaneously for both channels?
if yes, could you give me some notes who can assign profile and SDIO_x pins to do this?
regards
GenevaCooper - Moved from How to Use EngineerZone to Direct Digital Synthesis (DDS). Post date updated from Wednesday, January 22, 2025 9:26 PM UTC to Wednesday, January 22, 2025 9:27 PM UTC to reflect the move.
Hi basyouni ,
Apologies but it is not possible to perform frequency sweep and phase modulation simultaneously for both channels.
All the best,
Jules

Hi basyouni ,
The table only discusses that when using linear sweep, FR1[9:8] should be set to 00. Not because they can be used simultaneously with any modulation (frequency, amplitude, phase).
All the best,
Jules
Hi JULES
Thanks
Regards