Hi,
What are the steps for programming EVAL-AD9959 using SPI?
I referred the SINGLE-TONE MODE steps from datasheet [Rev. C | Page 19 of 44] and also Ref clock section from Page 20.
I am following below steps:
Step 1: Master_reset pulse for few microsec
Step 2: Enable all channels SPI 8 bits: HEX format
Reg 00 Data F0
Step 3: Set Ref clock:(25 MHz)
Reg 01 Data: D0 00 20
Step 4: Set Ouput Freq (5 MHz)
Reg 04 Data: 02 8F 5C 29
Step 5: Set Phase (0 deg)
Reg 05 Data: 00 00
Step 6: Send IO update pulse
But I don't see any output from the board.
Please help